Hello
We are having a custom am335x board, based on BBB, and we are facing an issue with the Ethernet controller.
When we are plugging in the ethernet cable, the leds on the connector seems to have some activity (blinking) but
nothing else.
The ethernet transceivers we are using is a Microchip LAN8710A-EZC-TR
eth0 Link encap:Ethernet HWaddr 84:eb:18:94:30:86 inet6 addr: fe80::86eb:18ff:fe94:3086/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:5 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:398 (398.0 B) Interrupt:56
Do you have any hint, or any tool that i can use to debug this issue?
Thank you in advance
Panos