Dear All,
We would face booting issues while we bring up the custom board, we are using our own custom board with AM3354 sitar processor.
I am following UART boot mode using minicom.
Setting SYSBOOT[15-0] configure according to UART boot configure.
After switch on the board we are getting on terminal CCCCCCCC characters appear on minicom window. from the minicomselected XMODEM and transfer
select "u-boot-spl.bin-am335x-evm" file or MLO file i tried both its loading successfully.
After image is successfully downloaded, the ROM code will boot, but i am not getting CCCCCC characters on the minicom terminal.
And i am not able load U-boot.img using YMODEM.
its giving time out error on minicom terminal.
i dont no where is the problem ... please suggest where i am hanging