Hi,
I have a customer in the bay area with a question regarding overdriving the Sitara clock lines. Please see below. Any comments are greatly appreciated!
The short of it is that customer is concerned about overdriving the crystal which has a 100 microwatt MAX spec. By changing the 330 ohm series resistor to 0, we risk overdriving if there is no current limiting function inside the Sitara. So can you verify that there is a current limiting feature within the Sitara and that we have no issue with overdrive? Also does the Sitara ESR spec apply to the raw crystal, or to the whole crystal circuit?
Thanks in advance,
Wally