Hi,
There are following mentions in the technical reference manual of AM5718.
Table 26-9. SATA PHY Tuning Table
Table 26-17. USB3 PHY Tuning Table
It is Reserved when I refer to these Physical address in Table 2-3 L4_CFG Memory Map.
Is this an error in writing?
Physical address of TRM of AM5728 is like Reserved in the same.
Best Regards,
Shigehiro Tsuda