Hi!
I'm new to the TI multicore DSP world and I just got the EVMK2H board (Rev 4.0). I read the first parts of the user guide, installed CCSv6, and downloaded the latest MCSDK. I have trying to update the images on the board with the latest ones (coming along with the MCSDK) but it failed. I got an indication that the JTAG device had to be updated. I checked the version of the JTAG module and it's the XDS200 one. Since I was following the steps provided here: http://processors.wiki.ti.com/index.php/Program_EVM_UG
I went to the program_evm directory to use the given script and try and update the JTAG firmware. This step didn't trigger any error but as soon as I try to connect to the board with CCSv6 or to update it, I got stuck with the same error:
SEVERE: IcePick_D_0: Error initializing emulator: (Error -1056 @ 0x0) A firmware update is
recommended for the XDS2xx debug probe. For XDS200 probes, update the firmware using the xd
s2xx_conf utility found in the .../ccs_base/common/uscif/xds2xx directory of the CCS instal
lation. View the ReadMe.txt file there for instructions. For other XDS2xx variants, follow
the manufacturer's instructions for updating the firmware. (Emulation package 6.0.83.1)
SEVERE: Could not start server: DebugServer.1: IcePick_D_0: Error initializing emulator: (E
rror -1056 @ 0x0) A firmware update is recommended for the XDS2xx debug probe. For XDS200 p
robes, update the firmware using the xds2xx_conf utility found in the .../ccs_base/common/u
scif/xds2xx directory of the CCS installation. View the ReadMe.txt file there for instructi
ons. For other XDS2xx variants, follow the manufacturer's instructions for updating the fir
mware. (Emulation package 6.0.83.1)
Any help would be appreciated :)
Thanks,
Thomas.