Hi,
I am working on the 28335, using Sys/bios and was wondering how is choosen/configured the CPU Timer used by the OS.
Indeed, to reduce the component power consumption, I only want to turn on one CpuTimer.
- In the Data Manual, this is said that CPU Timer 2 is used.
- In this article, it is said that one of the 3 CPU timer is used (processors.wiki.ti.com/.../BIOS_for_the_28x
- In practice, OS is only running when CPU Timer 1 is activated.
Any idea?
Thanks