Other Parts Discussed in Thread: DM385
Hello. I want to create a project using the DaVinci SoC.
My original idea was to buy a schmartboard to create pin interfaces for the chip. Though i contacted schmartboard support and they told me that BGA chips are not supported yet but will be in the future.
So what are my options now?
Is there a way to create the pcb using software, printing it somehow (if it is two layer), then do the BGA soldering on my own (i have equipment to do it manually)?
Or can i order a pcb for this chip from and online pcb manufacturer then solder the BGA chip?
Anyone interfaced with the Davinci? If yes, how you did it?
The less time consuming method is the best, as i want to get my hands on it asap!
Thanks!