Other Parts Discussed in Thread: SYSBIOS
I am trying to run OPUS encoder on C6748, however the process function of the encoder returns exception (opcode).
I thought the the opus codec library should be compatible with C6748 as well as mentioned in one of the forums.
The library specifically mentions C66xx compatible. COuld anyone from TI look into the below issue.
Can anyone point me to OPUS code so that i can compile it for C6748 without linking the library.
[C674X_0] Test Vector No. 1
Encoder Input : ..\TestVecs\Input\sample.wav
Encoder Reference Output : ..\TestVecs\Bitstream\sample_audio_48k_mono_128kbps_FB_c3.bit
Encoding 48000 Hz input at f kb/s in fullband mode with 480-sample frames.
Processing the frame: 1
A0=0x1 A1=0x0
A2=0x0 A3=0xc3056f38
A4=0x0 A5=0x0
A6=0x0 A7=0x0
A8=0x168 A9=0x168
A10=0xc3082040 A11=0xc305fcb8
A12=0xc3056f10 A13=0x15
A14=0x78 A15=0x1
A16=0x168 A17=0x6fc
A18=0xffffff88 A19=0xffe0b76e
A20=0x1e0 A21=0xc303e520
A22=0xc3057090 A23=0x1
A24=0x2 A25=0xc3004180
A26=0x450 A27=0x0
A28=0x51eb851f A29=0x30
A30=0x0 A31=0x2f
B0=0x1 B1=0x0
B2=0x80000000 B3=0xc3000440
B4=0x0 B5=0x0
B6=0x168 B7=0x0
B8=0x0 B9=0x1
B10=0x271a B11=0x1
B12=0xc30830f8 B13=0x4fb
B14=0xc30857d8 B15=0xc307cec8
B16=0x0 B17=0x1
B18=0x800 B19=0x1c9411
B20=0xffffff96 B21=0xffffff96
B22=0xffffff96 B23=0xffcb6204
B24=0xffcb2204 B25=0xffcb2a04
B26=0x1e0 B27=0xc305fbe0
B28=0xa0 B29=0x0
B30=0x0 B31=0x4fb
NTSR=0x1400c
ITSR=0x0
IRP=0x0
SSR=0x10
AMR=0x0
RILC=0x1
ILC=0x52
Exception at 0xc30004aa
EFR=0x2 NRP=0xc30004aa
Internal exception: IERR=0x8
Opcode exception
ti.sysbios.family.c64p.Exception: line 256: E_exceptionMax: pc = 0xc30004aa, sp = 0xc307cec8.
xdc.runtime.Error.raise: terminating execution