Other Parts Discussed in Thread: AM5728
Hi,
I would like to configure console to USB or UARTx on a custom hardware based on AM5728 core. Need help to achieve this.
Regards,
Srinidhi S.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM5728
Hi,
I would like to configure console to USB or UARTx on a custom hardware based on AM5728 core. Need help to achieve this.
Regards,
Srinidhi S.
Hi,
Default debug UART on AM335X AM57X is UART3. This should be enabled by default in the Linux SDK.
Hi,
I am referring to the latest TISDK: ti-processor-sdk-linux-am57xx-evm-02.00.01.07 & AM57xx GP EVM.
First you need to perform the appropriate pinmux settings & call the uartX init function in u-boot, in order to initialize the uart you want to use.
Then change the #define CONSOLEDEV in include/configs/am57xx_evm.h. Currently it is set to:
#define CONSOLEDEV "ttyO2"
Which as Biser already explained points to UART3.
In linux kernel, you need to:
1. Do the correct pinmux in am57xx-beagle-x15.dts
2. In am57xx-beagle-x15 add the following node:
&uartX {
status = "okay";
interrupts-extended = <set/interrupts>;
};
This should change your default console settings.
Best Regards,
Yordan