The TI Pin Mux Tool (http://www.ti.com/tool/pinmuxtooldoes not allow mixing different signal types between ports. Is this a software limitation of the tool, or a hardware limitation of the chip?
For example (in ZCZ package), would it be possible to use this configuration in the table below for Multi-Channel Audio, but set B13 as SPI1_D0, and use pin U16 for MCASP0_FSX?
PIN Name | PIN | Signal Name |
MCASP0_AHCLKX | A14 | mcasp0_ahclkx |
MCASP0_ACLKX | A13 | mcasp0_aclkx |
MCASP0_FSX | B13 |
|
MCASP0_AXR0 | D12 | mcasp0_axr0 |
MCASP0_AHCLKR | C12 | mcasp0_ahclkr |
MCASP0_ACLKR | B12 | mcasp0_aclkr |
MCASP0_FSR | C13 | mcasp0_fsr |
MCASP0_AXR1 | D13 | mcasp0_axr1 |
Thank you,
Phillip Do