The datasheet for AM335x talks about support for Device Boundary Scan and IEEE 1500. I'm wondering if the device has any built-in self test (BIST) instrumentation that can be controlled through the JTAG interface in order to run a memory test on externally connected DDR3 memory. Either through special test data registers directly accessible via the JTAG interface, or through IEEE 1500?