Hi,
We are using TDA2x Vayu board and Vision_SDK_02_07 for our application.
We have gone through "spry147.pdf". It is mentioned that "On the C66x CPU, customers can choose to execute fixed or floating point on an instruction by nstruction basis as the fixed- and floating point capability is fully integrated".
1. How do we configure instruction by instruction as float ?
2. We have a floating point version of our algorithm which is ported in the TDA2x platform. How can we know which instuction set(either fixed or float or combination) is getting used ?
3. Is there any compiler option to be added/changed for choosing floating point instruction set for a particular module or function ?
Thanks in advance.
Regards,
Niranjana A