This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NANDWriter_ARM Project

Other Parts Discussed in Thread: OMAP-L138

All:

LCDK138 board

XDS100v2 JTAG

CCS 6.1.1

OMAP-L138_FlasnAndBootUtils_2_40

Compiler version: TI v15.12.0.LTS

Output format: eabi (ELF)

I am trying to get the NANDWriter_ARM project running on the low-cost development board, but I am running into a problem:

#10008-D cannot find file "rtsv5_T_le_eabi.lib" 

 

Is there another library file that should be referenced?

Is the library file that is being sought in the OMAP-L138_FlasnAndBootUtils_2_40 directory?