Other Parts Discussed in Thread: AM3359
Hi ,
I am using am3359 ICEv2,
- Code Composer Studio version CCS 5.5
- SYSBIOS 6.41.00.26 Real Time Operating System
- XDC 3.30.05.60
- Compiler version TI v5.1.13
- Network Development Kit (NDK) 2.24.01.18
I am trying to run the enet_lwip example. I am using a sd card. I have the ethernet from my PC connected to the eth0. The jumper pins are shorting pins 1 and 2. When I open a browser for the website to show up at 192.168.1.2 it doesnt connect. when I do IPCONFIG on the pc the ip address on the port where the board is connected shows IP address 169....
I am a newbie. Can you please tell me what I am doing wrong here. The subnet is the same for both board and the pc.
Thank you