This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to insert the interrupt vector table in a C6202 DSP/BIOS confige file?

I use a DM642 board with a C6202 DSP/BIOS confige file for some reason. Now I need to open the interrupt GPIO_Interrupt_0 in DM642, which is not shown in C6202 DSP/BIOS confige file. What should I do to achieve this functionality?

I used to use the function C64_plug, but I can't debug it. The error code shows that C64_plug is a undefined symbol. How to use C64_plug correctly?

Thank you very much for you support. I am on-line waiting for reply.