Hi,ALL
I use DM365.
The memory rate ratio of application was seen by the "top" command.
Then, my application(adp_demo) displayed "102.2".
Since it is a ratio, I feel that it is unusual that "102.2" is shown.
I think that 100 or less is correct.
However, application is operating normally.
Someone,Please give me a view about the number of this "102.2".
Best Regard,
Ohsawa
-----------------------------------------------------------------------------------------------------------------
Welcome to MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921).
login[648]: root login on 'console'
# top
Mem: 57752K used, 15016K free, 0K shrd, 0K buff, 4980K cached
Load average: 0.52 0.37 0.15
PID USER STATUS VSZ PPID %CPU %MEM COMMAND
674 root RW 3040 648 1.9 4.1 top
647 root SW 74460 1 0.0 102.2 adp_demo
619 root SW 3112 1 0.0 4.2 inetd
648 root SW 3040 1 0.0 4.1 sh
611 bin SW 1712 1 0.0 2.3 portmap
330 root SW< 1572 1 0.0 2.1 udevd
1 root SW 1552 0 0.0 2.1 init
13 root SW< 0 1 0.0 0.0 khelper
11 root SW< 0 1 0.0 0.0 desched/0
2 root SW 0 1 0.0 0.0 posix_cpu_timer
3 root SW 0 1 0.0 0.0 softirq-high/0
4 root SW 0 1 0.0 0.0 softirq-timer/0
5 root SW 0 1 0.0 0.0 softirq-net-tx/
6 root SW 0 1 0.0 0.0 softirq-net-rx/
7 root SW 0 1 0.0 0.0 softirq-block/0
8 root SW 0 1 0.0 0.0 softirq-tasklet
9 root SW 0 1 0.0 0.0 softirq-hrtimer
10 root SW 0 1 0.0 0.0 softirq-rcu/0
12 root SW< 0 1 0.0 0.0 events/0
14 root SW< 0 1 0.0 0.0 kthread
26 root SW< 0 14 0.0 0.0 kblockd/0Mem: 57764K used, 15004K free, 0K shrd, 0K buff, 4980K cached