This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB_Stick_Sample

Other Parts Discussed in Thread: CCSTUDIO

I am using CCSV4.1.2 and attempting to import and build the USB_Stick_Sample from:

http://support.spectrumdigital.com/boards/usbstk5515/reva/

I have had issues importing this (possibly due to macros.ini - thanks to SD for keeping things simple) but have added include paths to compiler build settings.  The compiler is looking for system_drv.h but can not find it.  I have searched my entire drive and I can not find this either.

Where should system_drv.h be?  I have tried commenting out the #include from i2s_sample.c but this generates more errors so I guess it is required.

Here is the compiler log:

C:\CCStudio_v4.1.2\ccsv4\utils\gmake\gmake -k all

asm/subdir.mk:51: warning: overriding commands for target `vector.obj'

src/subdir.mk:139: warning: ignoring old commands for target `vector.obj'

'Building file: ../src/i2s_sample.c'

'Invoking: Compiler'

"C:/CCStudio_v4.1.2/ccsv4/tools/compiler/c5500/bin/cl55" -vcpu:3.3 -g --define="_DEBUG" --define="C55X" --include_path="C:/CCStudio_v4.1.2/ccsv4/tools/compiler/c5500/include" --include_path="C:/CCStudio_v4.1.2/c55xx_csl/inc" --include_path="../inc" --include_path="C:/CCS4Work/Projects/usbstk5515bsl/include" --include_path="C:/CCS4Work/Projects/EZDSP_Sample V0.0/Debug" --include_path="C:/CCStudio_v4.1.2/bios_5_41_02_14/packages/ti/bios/include" --include_path="C:/CCStudio_v4.1.2/bios_5_41_02_14/packages/ti/rtdx/include/c5500" --diag_warning=225 --ptrdiff_size=32 --algebraic --memory_model=large --asm_source=algebraic --preproc_with_compile --preproc_dependency="src/i2s_sample.pp" "../src/i2s_sample.c"

"../src/i2s_sample.c", line 44: fatal error: could not open source file "system_drv.h"

1 fatal error detected in the compilation of "../src/i2s_sample.c".

Compilation terminated.

Regards, Andrew

  • I have realised that this example can not be copied in to the workspace with CCSV4 because some of the project build information goes missing.

    If I import this without copying it builds and runs ok.

    In most (all?) of the other IDEs I have used I would have reported this as a bug.....

    Regards, Andrew