This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

beaglebone black u-boot optimization



Hi,

In below, debian flasher emmc image u-boot.img and MLO output. I want to minimize (now it boots at 2.621 seconds). Currently I suppose that 1sc bootdelay when u-boot is opening, how can I close it?

0.000 0.000:
0.000 0.000: U-Boot SPL 2015.07 (Oct 07 2015 - 14:27:57)
0.000 0.000: reading args
0.066 0.066: spl_load_image_fat_os: error reading image args, err - -1
0.066 0.000: reading u-boot.img
0.066 0.000: reading u-boot.img
0.066 0.000:
0.066 0.000:
U-Boot 2015.07 (Oct 07 2015 - 14:27:57 -0400)
0.276 0.000:
       Watchdog enabled
I2C:   ready
DRAM:  512 MiB
NAND:  0 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
0.367 0.000:
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
0.514 0.000:
Net:   <ethaddr> not set. Validating first E-fuse MAC
Phy 0 not found
cpsw, usb_ether
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
783 bytes read in 9 ms (85 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
switch to partitions #0, OK
mmc1(part 0) is current device
switch to partitions #0, OK
mmc0 is current device
3232496 bytes read in 277 ms (11.1 MiB/s)
Booting from external microSD...
32990 bytes read in 98  (328.1 KiB/s)
## Error: "mmcargs" not defined
Kernel image @ 0x82000000 [ 0x000000 - 0x3152f0 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8fff4000, end 8ffff0dd ... OK
2.621 0.000:

my rootfs is:

arago_base_sdk

my uEnv.txt is:

optargs=
loadfdt=load mmc ${mmcdev}:2 ${fdtaddr} /boot/dtbs/${fdtfile}


loaduimage=mw.l 4804c134 fe1fffff; if load mmc 0:2 ${loadaddr} /boot/zImage; the
n setenv mmcdev 0; mw.l 4804c194 01200000; echo Booting from external microSD...
; else setenv mmcdev 1; if test $mmc0 = 1; then setenv mmcroot /dev/mmcblk1p2 rw
; fi; load mmc 1:2 ${loadaddr} /boot/zImage; mw.l 4804c194 00c00000; echo Bootin
g from internal eMMC...; fi


mmcboot=run mmcargs; bootz ${loadaddr} - ${fdtaddr}


uenvcmd=i2c mw 0x24 1 0x3e; run findfdt; if test $board_name = A335BNLT; then se
tenv mmcdev 1; mmc dev ${mmcdev}; if mmc rescan; then setenv mmc1 1; else setenv
 mmc1 0; fi; fi; setenv mmcdev 0; mmc dev ${mmcdev}; if mmc rescan; then setenv
mmc0 1; else setenv mmc0 0; fi; run loaduimage && run loadfdt && run mmcboot

 


There are some errors and warnings on u-boot as you seen,

1) 0.066 0.066: spl_load_image_fat_os: error reading image args, err - -1

2) ** Unable to read "uboot.env" from mmc0:1 **

3) ** Unable to read file boot.scr **

4) Error: "mmcargs" not defined


how can I fix them?

Is there any way to optimize u-boot? (I also read sitara boot time reduction wiki but it doenst help me)

Best Regards,

Umit