Hi,
I have done a program about the TMS320vc5402, and it's can do well by CCS2.2. Because I want run it in CCS3.3, I must transplant the program.
I used the CPU is TMS320vc5402, and the CPU connect with an external RAM and an external nand flash.
I want to burn the programs into the nand flash. I have 3 projects, one is to burn the word stock into the flash, one is used to burn the application program into the flash, the other one is my application program. The application program is modified and it can debug well.
At last, I want to burn the word stock and the application program into the flash.By doing this, I have some questions. I couldn't burn it ! But use CCS2.2, it do well. I tried to modify the gel and programs, but I don't know how to modify. Try many ways, it's not right.
May I ask for you to get a routine about the gel and a project to burn the application program? Or give me some advice.(note: external RAM and external flash. The register value about PMST is 0xffc0).
Thank you very much.
Best regards.