This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to set the C5515 System Clock in CCSV4 Bios Project

I am used to a CCSV3.1 Bios project where I set CLKMD register statically via the global settings in the DSP/BIOS graphical configuration tool.

I am now using CCSV4 and have noticed that this setting (or C5515 equivalent) is missing from the CCSV4 DSP/BIOS .tcf configuration file.

How do I set up the PLL registers using CCSV4 BIOS project?

Is there an example of how this is done?

My custom hardware has a 12MHz external clock with the RTC disabled.

Regards, Andrew.