Hi, I'm working on an am335x project and I am trying to integrate an audio capture-only codec that acts as I2S master and produces sound in LEFT-J format. This codec has no audio controls over i2c. I've set up a dummy codec module that just accepts any parameter and is fixed to 16KHz, 16-bit LE, stereo audio. I've hooked that up to the davinci-evm module and added this DAI:
static struct snd_soc_dai_link input_dai_dummy_i2s = {
.name = "Dummy I2S Capture",
.stream_name = "Capture",
.codec_dai_name = "dummy-i2s",
.ops = &evm_ops,
.init = evm_dummy_i2s_init,
.dai_fmt = SND_SOC_DAIFMT_LEFT_J | SND_SOC_DAIFMT_CBM_CFM | SND_SOC_DAIFMT_NB_NF,
};
And I've updated the device tree IDs for my new codec:
static const struct of_device_id davinci_evm_dt_ids[] = {
{
.compatible = "ti,dummy-i2s-evm-audio",
.data = (void *) &input_dai_dummy_i2s,
},
{
.compatible = "ti,da830-evm-audio",
.data = (void *) &evm_dai_tlv320aic3x,
},
{ /* sentinel */ }
}
My evm_dummy_i2s_init is almost the same as the evm_aic3x_init function except I've removed the controls and non-connected pin registration:
static int evm_dummy_i2s_init(struct snd_soc_pcm_runtime *rtd)
{
struct snd_soc_card *card = rtd->card;
struct snd_soc_codec *codec = rtd->codec;
struct device_node *np = card->dev->of_node;
int ret;
if (np) {
ret = snd_soc_of_parse_audio_routing(card, "ti,audio-routing");
if (ret)
return ret;
} else {
/* Set up davinci-evm specific audio path audio_map */
snd_soc_dapm_add_routes(&card->dapm, audio_map,
ARRAY_SIZE(audio_map));
}
return 0;
}
Finally, I added some device tree nodes (in this reduced example I'm working on a beaglebone black) and removed all the HDMI connectivity. I also enabled mcasp in mode 3 so I can use P8's pins 33, 35, and 36.
/* * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/ * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ /dts-v1/; #include "am33xx.dtsi" #include "am335x-bone-common.dtsi" / { model = "TI AM335x BeagleBone Black"; compatible = "ti,am335x-bone-black", "ti,am335x-bone", "ti,am33xx"; }; &ldo3_reg { regulator-min-microvolt = <1800000>; regulator-max-microvolt = <1800000>; regulator-always-on; }; &mmc1 { vmmc-supply = <&vmmcsd_fixed>; }; &mmc2 { vmmc-supply = <&vmmcsd_fixed>; pinctrl-names = "default"; pinctrl-0 = <&emmc_pins>; bus-width = <8>; status = "okay"; }; &rtc { system-power-controller; }; &am33xx_pinmux { mcasp0_audio_input_pins: mcasp0_audio_input_pins { pinctrl-single,pins = < 0xd0 ( PIN_INPUT | MUX_MODE3 ) /* (V2) lcd_data12.mcasp0_aclkr */ 0xd4 ( PIN_INPUT | MUX_MODE3 ) /* (V3) lcd_data13.mcasp0_fsr */ 0xc8 ( PIN_INPUT | MUX_MODE3 ) /* (U3) lcd_data10.mcasp0_axr0 */ >; }; mcasp0_audio_input_pins_sleep: mcasp0_audio_input_pins_sleep { pinctrl-single,pins = < 0xd0 ( PIN_INPUT | MUX_MODE3 ) /* (V2) lcd_data12.mcasp0_aclkr */ 0xd4 ( PIN_INPUT | MUX_MODE3 ) /* (V3) lcd_data13.mcasp0_fsr */ 0xc8 ( PIN_INPUT | MUX_MODE3 ) /* (U3) lcd_data10.mcasp0_axr0 */ >; }; }; &mcasp0 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&mcasp0_audio_input_pins>; pinctrl-1 = <&mcasp0_audio_input_pins_sleep>; status = "okay"; op-mode = <0>; tdm-slots = <2>; serial-dir = < 2 0 0 0 >; rx-num-evt = <1>; tx-num-evt = <1>; }; / { dummy_i2s: dummy_i2s { compatible = "linux,dummy-i2s"; status = "okay"; }; sound@0 { compatible = "ti,dummy-i2s-evm-audio"; ti,model = "Dummy I2S"; ti,audio-codec = <&dummy_i2s>; ti,mcasp-controller = <&mcasp0>; ti,codec-clock-rate = <1024000>; ti,audio-routing = "ANA IN1", "Internal Mic"; }; };
Anyway, I'm running Linux 4.4.1 and the codec registers correctly after all this. However, when I try to record with arecord, it hangs indefinitely and no audio is produced to the output file. I can verify that the device is producing a 1024000 Hz bit clock and 16000 Hz frame sync clock. I have a 3-wire connection between the codec and my beaglebone with ACLKR, FSR, and AXR0 pins hooked up.
A representative from the codec maker has indicated that the codec does not need a master clock but maybe the mcasp/davinci-evm needs one when operating as slave. Does anyone have any experience in these cases?
Thanks.