This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

failed to load module: /usr/lib/gbm/gbm_dri.so:

Hi,

We have created the SD card using create-sdcard.sh from the path

/home/medha/ti-processor-sdk-linux-am57xx-evm-02.00.01.07/bin

if we run the kmscube

root@am57xx-evm:~# kmscube
trying to load module omapdrm...success.
### Display [0]: CRTC = 32, Connector = 30
        Mode chosen [800x480] : Clock => 33000, Vertical refresh => 60, Type => 72
        Horizontal => 800, 1010, 1040, 1056, 0
        Vertical => 480, 502, 515, 525, 0
### Primary display => ConnectorId = 30, Resolution = 800x480
failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file: No such file or directory
failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared object file: No such file or directory
loaded module: gbm_pvr.so
PVR:(Warning): PVRSRVOpenDCDevice: Warning - 138 returned [80, /bridged_pvr_dc_glue.c]
Using display 0x1 with EGL version 1.4
EGL Version "1.4 build 1.9@2253347"
EGL Vendor "Imagination Technologies"
EGL Extensions "EGL_IMG_client_api_ogl EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cu"
display 0 failed to set mode: Permission denied

root@am57xx-evm:/# weston
Date: 2016-01-09 UTC
[01:36:01.507] weston 1.6.0
               wayland.freedesktop.org/
               Bug reports to: bugs.freedesktop.org/enter_bug.cgi
               Build: 1.5.93-5-g2858cc2 configure.ac: bump version to 1.6.0 (2014-09-19 13:40:14 +0300)
[01:36:01.508] OS: Linux, 4.1.13-g8dc6617, #1 SMP PREEMPT Fri Jan 8 18:44:32 EST 2016, armv7l
[01:36:01.508] Using config file '/etc//weston.ini'
[01:36:01.508] Loading module '/usr/lib/weston/wayland-backend.so'
[01:36:01.508] Failed to load module: /usr/lib/weston/wayland-backend.so: cannot open shared object file: No such file or directory

Kindly suggest what might be the issue. Why we are getting these kind of issues in prebuilt images and with evm.

Thanks & Regards,

N.V.Subbaiah.