This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910A3 wrong VRTC



Hi

We have interfaced TPS65910A3A1RSL with AM3352BZCZ60 processor.

We are connecting the VRTC LDO output to the VDDS_RTC(D7) pin of the processorAM3352BZCZ60.

When  we are not powering on the PMIC we are noticing VDDS_RTC voltage going to 1.8V. But when we are powering on the PMIC we are noticing a voltage rise of 2.4V at the VDDS_RTC pin of the processor.

The other outputs of the PMIC are working fine.

Another point to be noted is
If we disconnect VRTC(of PMIC) then VRTC of PMIC comes back to 1.8V but VDDS_RTC of processor stays at2.4V.
How can VDDS_RTC source 2.4V when it is a power input pin?

Kindly help us on this issue.