This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiplier and divider value of AM437x DDR DPLL in Linux SDK

Guru 15520 points

Hi,

I have a question about DDR DPLL configuration in AM437x Linux SDK.

In Linux SDK version v07.01.00.00, multiplier and divider of DDR DPLL
for GP-EVM are setup as following:
************************************
[CLKINP=24MHz]
 M = 400
 N = 23
 M2 = 1
 M4 = 1
(These value will make DDR CLK to be 400MHz and DLL CLK to be 800MHz)
************************************

but in latest SDK version v02.00.01.07, it's setup as following:
************************************
[CLKINP=24MHz]
 M = 50
 N = 2
 M2 = 1
 M4 = 2
(These value will make DDR CLK to be 400MHz and DLL CLK to be 400MHz)
************************************

Why "M", "N", "M4" value been changed in the latest SDK?
Are there any reason for these changes?

best regards,
g.f.