Other Parts Discussed in Thread: DRA752, PMP, BEAGLEBOARD-X15, AM5728, TMP102, TLV320AIC3104, ASH
I am working on a custom system image and I got an aleatory kernel internal Oops error. The error occurs completely randomly, I can boot the board many times without presenting the error, but sometimes it appears just after booting while running udev. I will paste here my log information: The error is this:
[ 9.669062] Unable to handle kernel paging request at virtual address ffffffff
[ 9.902470] Internal error: Oops: 17 [#1] PREEMPT SMP ARM
[ 9.931682] CPU: 1 PID: 474 Comm: udevd Not tainted 4.1.6-g52c4aa7 #1
The completely log information is this one:
U-Boot SPL 2015.07-00114-g167724d-dirty (Feb 04 2016 - 16:06:54)
DRA752 ES1.1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2015.07-00114-g167724d-dirty (Feb 04 2016 - 16:06:54 -0600)
CPU : DRA752 ES1.1
Board: BeagleBoard x15
I2C: ready
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
162 bytes read in 3 ms (52.7 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
reading zImage
3076024 bytes read in 158 ms (18.6 MiB/s)
reading am57xx-beagle-x15.dtb
92484 bytes read in 9 ms (9.8 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x2eefb8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe6000, end 8ffff943 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.6-g52c4aa7 (dgarbanzo@ridgerun-GA-890FXA-UD5) (gcc version 4.8.2 20130603 (prerelease) (crosstool-NG 1.19.0 - Linaro GCC 2013.07) ) #1 SMP PREEMPT Wed Feb 3 17:10:45 CST 2016
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI AM5728 BeagleBoard-X15
[ 0.000000] Reserved memory: created CMA memory pool at 0x95800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x99000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9f000000, size 16 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0xfe400000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] DRA752 ES1.1
[ 0.000000] PERCPU: Embedded 12 pages/cpu @ee536000 s17088 r8192 d23872 u49152
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 481105
[ 0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/nfs nfsroot=10.251.101.4:/home/dgarbanzo/work/AM5728evm-RRSDK-Trunk-GIT/dgarbanzo-sdk-AM5728-trunk-new/fs/fs rw ip=dhcp
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1707288K/1931260K available (5719K kernel code, 282K rwdata, 2092K rodata, 320K init, 249K bss, 27364K reserved, 196608K cma-reserved, 1292284K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef800000 ( 760 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc07a9034 (7813 kB)
[ 0.000000] .init : 0xc07aa000 - 0xc07fa000 ( 320 kB)
[ 0.000000] .data : 0xc07fa000 - 0xc0840a88 ( 283 kB)
[ 0.000000] .bss : 0xc0843000 - 0xc08817fc ( 250 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32768 Hz
[ 0.000000] clocksource 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000030] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.000030] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000427] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000457] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000462] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000473] Switching to timer-based delay loop, resolution 162ns
[ 0.001031] Console: colour dummy device 80x30
[ 0.001049] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.001056] This ensures that you still see kernel messages. Please
[ 0.001062] update your kernel commandline.
[ 0.001075] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.001088] pid_max: default: 32768 minimum: 301
[ 0.001167] Security Framework initialized
[ 0.001203] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001214] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001764] Initializing cgroup subsys blkio
[ 0.001778] Initializing cgroup subsys memory
[ 0.001805] Initializing cgroup subsys devices
[ 0.001818] Initializing cgroup subsys freezer
[ 0.001830] Initializing cgroup subsys perf_event
[ 0.001853] CPU: Testing write buffer coherency: ok
[ 0.002113] /cpus/cpu@0 missing clock-frequency property
[ 0.002166] /cpus/cpu@1 missing clock-frequency property
[ 0.002177] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002217] Setting up static identity map for 0x80008280 - 0x800082d8
[ 0.060724] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.060787] Brought up 2 CPUs
[ 0.060800] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.060806] CPU: All CPU(s) started in SVC mode.
[ 0.061200] devtmpfs: initialized
[ 0.086568] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.087324] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.100378] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.100832] omap_hwmod: tptc1 using broken dt data from edma-controller
[ 0.272229] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.276674] pinctrl core: initialized pinctrl subsystem
[ 0.277518] NET: Registered protocol family 16
[ 0.278427] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.300609] cpuidle: using governor ladder
[ 0.330633] cpuidle: using governor menu
[ 0.337130] OMAP GPIO hardware version 0.1
[ 0.342404] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.364459] No ATAGs?
[ 0.364492] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.364501] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.367052] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.367062] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.367550] OMAP DMA hardware revision 0.0
[ 0.408656] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.411382] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.416403] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.416575] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.416733] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.416883] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.417145] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.417315] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.417544] vgaarb: loaded
[ 0.417941] SCSI subsystem initialized
[ 0.419071] palmas 0-0058: Irq flag is 0x00000008
[ 0.432539] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[ 0.514564] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.515125] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.515339] pps_core: LinuxPPS API ver. 1 registered
[ 0.515347] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.515376] PTP clock support registered
[ 0.515970] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 0.516254] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 0.516537] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.516817] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.517097] Advanced Linux Sound Architecture Driver Initialized.
[ 0.517748] Switched to clocksource arch_sys_counter
[ 0.527021] NET: Registered protocol family 2
[ 0.527562] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.527626] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.527776] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.527827] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.527858] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.528003] NET: Registered protocol family 1
[ 0.528232] RPC: Registered named UNIX socket transport module.
[ 0.528241] RPC: Registered udp transport module.
[ 0.528248] RPC: Registered tcp transport module.
[ 0.528255] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.529249] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[ 0.529285] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.531099] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.531178] audit: initializing netlink subsys (disabled)
[ 0.531209] audit: type=2000 audit(0.510:1): initialized
[ 0.537257] VFS: Disk quotas dquot_6.6.0
[ 0.537422] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.539408] NFS: Registering the id_resolver key type
[ 0.539435] Key type id_resolver registered
[ 0.539443] Key type id_legacy registered
[ 0.539496] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.541536] NET: Registered protocol family 38
[ 0.541619] bounce: pool size: 64 pages
[ 0.541767] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250)
[ 0.541781] io scheduler noop registered
[ 0.541793] io scheduler deadline registered
[ 0.541827] io scheduler cfq registered (default)
[ 0.545373] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 0.579755] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 0.579768] pci_bus 0000:00: root bus resource [io 0x1000-0xffff]
[ 0.579780] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.579791] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.579894] pci 0000:00:00.0: IOMMU is currently not supported for PCI
[ 0.580170] PCI: bus0: Fast back to back transfers disabled
[ 0.580296] PCI: bus1: Fast back to back transfers enabled
[ 0.580388] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.580404] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.580417] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.583802] OMAP DSS rev 6.1
[ 0.584067] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 0.584604] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[ 0.588535] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.591511] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 299, base_baud = 3000000) is a 8250
[ 1.551979] console [ttyS2] enabled
[ 1.556646] [drm] Initialized drm 1.1.0 20060810
[ 1.569909] brd: module loaded
[ 1.577240] loop: module loaded
[ 1.581397] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.591002] mousedev: PS/2 mouse device common for all mice
[ 1.596605] i2c /dev entries driver
[ 1.601608] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.606480] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr104 mode
[ 1.612974] omap_hsmmc 4809c000.mmc: no pinctrl state for hs200_1_8v mode
[ 1.619814] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr50 mode
[ 1.626196] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr50 mode
[ 1.632603] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr25 mode
[ 1.639006] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr12 mode
[ 1.645387] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr_1_8v mode
[ 1.688407] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr104 mode
[ 1.694878] omap_hsmmc 480b4000.mmc: no pinctrl state for hs200_1_8v mode
[ 1.701732] omap_hsmmc 480b4000.mmc: no pinctrl state for ddr50 mode
[ 1.708134] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr50 mode
[ 1.714516] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 1.720909] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 1.727482] vdd_3v3: supplied by regen1
[ 1.766666] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.768115] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.768446] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 1.787097] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 1.790030] mmc0: new high speed SDHC card at address aaaa
[ 1.790350] mmcblk0: mmc0:aaaa SL08G 7.40 GiB
[ 1.793855] mmcblk0: p1
[ 1.805873] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 1.812627] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 1.821697] davinci-mcasp 48468000.mcasp: ERRATA i868 workaround is enabled
[ 1.829915] oprofile: using timer interrupt.
[ 1.834418] Initializing XFRM netlink socket
[ 1.838748] NET: Registered protocol family 17
[ 1.842403] mmc1: MAN_BKOPS_EN bit is not set
[ 1.847606] NET: Registered protocol family 15
[ 1.851243] mmc1: new DDR MMC card at address 0001
[ 1.851572] mmcblk1: mmc1:0001 S10004 3.56 GiB
[ 1.851706] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB
[ 1.851818] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB
[ 1.852487] mmcblk1: p1 p2 p3
[ 1.876576] Key type dns_resolver registered
[ 1.880980] omap_voltage_late_init: Voltage driver support not added
[ 1.887606] Power Management for TI OMAP4+ devices.
[ 1.892787] ThumbEE CPU extension supported.
[ 1.897090] Registering SWP/SWPB emulation handler
[ 1.903357] dmm 4e000000.dmm: workaround for errata i878 in use
[ 1.911188] dmm 4e000000.dmm: initialized all PAT entries
[ 1.920051] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.926695] [drm] No driver support for vblank timestamp query.
[ 2.201434] [drm] Enabling DMM ywrap scrolling
[ 2.217659] Console: switching to colour frame buffer device 160x45
[ 2.233871] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.239833] omapdrm omapdrm.0: registered panic notifier
[ 2.267776] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.317768] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 2.323893] davinci_mdio 48485000.mdio: detected phy mask fffffff9
[ 2.334378] libphy: 48485000.mdio: probed
[ 2.338431] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver unknown
[ 2.346471] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 2.355141] cpsw 48484000.ethernet: Detected MACID = 74:da:ea:47:b8:d2
[ 2.362438] cpsw 48484000.ethernet: cpsw: Detected MACID = 74:da:ea:47:b8:d3
[ 2.370119] hctosys: unable to open rtc device (rtc0)
[ 2.387391] net eth0: initializing cpsw version 1.15 (0)
[ 2.471923] net eth0: phy found : id is : 0x221622
[ 2.481422] net eth1: initializing cpsw version 1.15 (0)
[ 2.571763] net eth1: phy found : id is : 0x221622
[ 4.474970] cpsw 48484000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 4.497759] Sending DHCP requests ., OK
[ 4.567759] IP-Config: Got DHCP answer from 10.251.101.1, my address is 10.251.101.95
[ 4.579783] IP-Config: Complete:
[ 4.583029] device=eth0, hwaddr=74:da:ea:47:b8:d2, ipaddr=10.251.101.95, mask=255.255.255.0, gw=10.251.101.1
[ 4.593361] host=10.251.101.95, domain=cr.ridgerun.com, nis-domain=(none)
[ 4.600658] bootserver=10.251.101.1, rootserver=10.251.101.4, rootpath=
[ 4.607562] nameserver0=200.91.75.5, nameserver1=8.8.8.8
[ 4.613759] ldousb: disabling
[ 4.617013] aic_dvdd_fixed: disabling
[ 4.620948] ALSA device list:
[ 4.623927] No soundcards found.
[ 4.631625] VFS: Mounted root (nfs filesystem) on device 0:15.
[ 4.637839] devtmpfs: mounted
[ 4.641070] Freeing unused kernel memory: 320K (c07aa000 - c07fa000)
starting pid 86, tty '': '/etc/rcS'
loading modules
no /etc/modules, exiting
Starting System
done.
Welcome to
__________ .__ .___ __________
\______ \|__| __| _/ ____ ____ \______ \ __ __ ____
| _/| | / __ | / ___\ _/ __ \ | _/| | \ / \
| | \| |/ /_/ | / /_/ >\ ___/ | | \| | /| | \
|____|_ /|__|\____ | \___ / \___ >|____|_ /|____/ |___| /
\/ \//_____/ \/ \/ \/
Embedded Linux Solutions
For further information see:
http://www.ridgerun.com
Build host: ridgerun-GA-890FXA-UD5
Built by: dgarbanzo
Build date: Fri, 05 Feb 2016 11:18:55 -0600
Build tag: am5728-tievm
Configuring network interfaces
Starting D-Bus message bus system
[ 5.373459] random: dbus-daemon urandom read with 87 bits of entropy available
Starting udev
[ 5.469925] udevd[166]: starting version 182
[ 5.749187] random: nonblocking pool is initialized
[ 8.983284] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc2
[ 9.379745] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 9.412568] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 9.456276] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
[ 9.503598] omap-rproc 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
[ 9.524290] media: Linux media interface: v0.10
[ 9.559702] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
[ 9.601392] remoteproc0: 58820000.ipu is available
[ 9.669062] Unable to handle kernel paging request at virtual address ffffffff
[ 9.708201] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
[ 9.735154] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 9.802775] pgd = ebc74000
[ 9.863424] nfs: RPC call returned error 14
[ 9.863653] Linux video capture interface: v2.00
[ 9.873344] [ffffffff] *pgd=af7aa821
[ 9.883436] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
[ 9.898245] , *pte=00000000, *ppte=00000000
[ 9.902470] Internal error: Oops: 17 [#1] PREEMPT SMP ARM
[ 9.907892] Modules linked in: videodev libata phy_omap_usb2 media omap_remoteproc(+) cpufreq_voltdm(+) remoteproc omap_rng omap_wdt ti_soc_thermal snd_soc_simple_card dwc3_omap rng_core rtc_omap virtio thermal_sys extcon_usb_gpio virtio_ring extcon leds_gpio hwmon
[ 9.931682] CPU: 1 PID: 474 Comm: udevd Not tainted 4.1.6-g52c4aa7 #1
[ 9.938151] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 9.944275] task: ecef3700 ti: ecefc000 task.ti: ecefc000
[ 9.949709] PC is at find_get_entry+0x34/0xb4
[ 9.954091] LR is at 0x0
[ 9.956637] pc : [<c00c1598>] lr : [<00000000>] psr: a0000113
[ 9.956637] sp : ecefdc10 ip : ffffffff fp : ecefdc2c
[ 9.968167] r10: 00000000 r9 : c084028c r8 : 00000000
[ 9.973413] r7 : edd69650 r6 : 00000000 r5 : 00000000 r4 : 00000000
[ 9.979967] r3 : ecefdbfc r2 : 00000000 r1 : 00000000 r0 : ffffffff
[ 9.986525] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 9.993869] Control: 10c5387d Table: abc7406a DAC: 00000015
[ 9.999640] Process udevd (pid: 474, stack limit = 0xecefc218)
[ 10.005497] Stack: (0xecefdc10 to 0xecefe000)
[ 10.009873] dc00: 00000000 00000000 00000000 edd6964c
[ 10.018086] dc20: ecefdc5c ecefdc30 c00c16b4 c00c1570 00000000 00000000 00000000 00000001
[ 10.026301] dc40: edd6964c ed1b2780 00000000 00000000 ecefdcd4 ecefdc60 c00c2ac8 c00c1694
[ 10.034515] dc60: c010d114 c010ce90 ecefdce0 ed1b2780 00000001 ed1b27e8 00000000 edd69570
[ 10.042732] dc80: 00000fff ffffffff ecefdd0c ecefdd20 ecefdcc4 ecefdca0 c01e91b0 c059955c
[ 10.050949] dca0: ecefdd20 edd69570 ecefdd0c ecefdd20 edd69570 ecefdd0c ecefdd98 00000080
[ 10.059164] dcc0: ed2bc919 ebd23948 ecefdcf4 ecefdcd8 c01e6958 c00c2928 c01e6904 00000000
[ 10.064949] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.077072] remoteproc0: Direct firmware load for dra7-ipu1-fw.xem4 failed with error -2
[ 10.077075] remoteproc0: Falling back to user helper
[ 10.091036] dce0: 00000000 ed1b2780 ecefdd64 ecefdcf8 c0104b34 c01e6910 00000080 c0139c2c
[ 10.099250] dd00: 00000000 ed733600 00000080 00000002 00000000 00000080 ecefdd04 00000001
[ 10.107463] dd20: ed1b2780 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 10.115676] dd40: ed1b2780 ed1b2780 ed733600 ecefdd98 ed1b2780 c08136cc ecefdd94 ecefdd68
[ 10.123890] dd60: c01051cc c0104a90 c010e054 c026ccc4 bf000000 ed733600 00000000 ed1b2780
[ 10.132101] dd80: c08136cc ed2bc919 ecefddb4 ecefdd98 c0109d20 c0105154 00000000 00000000
[ 10.140314] dda0: 00000000 ec93b600 ecefde3c ecefddb8 c01489a0 c0109cf0 ed733600 00000080
[ 10.148527] ddc0: 00000080 ecc0cc08 00000001 ecefddb8 00000000 ebd23948 ecefde14 ecefdde8
[ 10.156739] dde0: c0105228 ebe52500 00000000 00000000 bf000000 edd68dd8 ed2bc900 00000001
[ 10.164950] de00: c08136cc c08136cc ecefde34 ecefde18 c0109d20 ed733600 c0813bc4 fffffff8
[ 10.173163] de20: 00000001 c08136cc c08136cc ebd23948 ecefde64 ecefde40 c010ab04 c014880c
[ 10.181375] de40: ed733600 00000000 fffffff8 00000001 c08136cc c08136cc ecefdf04 ecefde68
[ 10.189588] de60: c0148388 c010aa94 00000000 ed733602 6e69622f 0068732f 00000000 c085f338
[ 10.197800] de80: befff00f 0000001d ecefdebc ecefde98 c00e0e70 c05995b4 00000b14 ef6ebf50
[ 10.206013] dea0: 00000000 beffff1f befff000 0000001d ecefded4 ecefdec0 c00e0f3c c059955c
[ 10.214225] dec0: 00000440 ef6ebf50 ecefdee4 ecefded8 c001e228 c00e0ec8 ecefdf2c ecefdee8
[ 10.222438] dee0: ed733600 c0813b28 fffffffe 00000001 ed733600 c0813ba8 ecefdf2c ecefdf08
[ 10.230649] df00: c010ab04 c0148198 ed733600 ecef3700 00000000 ebd19000 000001da ec9db500
[ 10.238861] df20: ecefdf74 ecefdf30 c010b2f8 c010aa94 ebd19000 ec9db538 0003f7e0 be8563e8
[ 10.247073] df40: 00000000 ecef3980 c0112338 0003f7e0 be8563e8 00000005 0000000b c000f204
[ 10.255286] df60: ecefc000 00000000 ecefdf8c ecefdf78 c010b4d8 c010aef8 00000000 c0112300
[ 10.263499] df80: ecefdfa4 ecefdf90 c010b728 c010b4b0 00027008 ffffffff 00000000 ecefdfa8
[ 10.271711] dfa0: c000f060 c010b710 00027008 ffffffff be8565e8 be8563e8 0003f7e0 00000008
[ 10.279924] dfc0: 00027008 ffffffff 00000005 0000000b 00026464 0003f7e0 ffffffff 0001a0f1
[ 10.288137] dfe0: 0000000b be856334 b6e52d43 b6df9716 80000030 be8565e8 4d4f5246 5645445f
[ 10.296346] Backtrace:
[ 10.298819] [<c00c1564>] (find_get_entry) from [<c00c16b4>] (pagecache_get_page+0x2c/0x198)
[ 10.307203] r7:edd6964c r6:00000000 r5:00000000 r4:00000000
[ 10.312926] [<c00c1688>] (pagecache_get_page) from [<c00c2ac8>] (generic_file_read_iter+0x1ac/0x5cc)
[ 10.322095] r10:00000000 r9:00000000 r8:ed1b2780 r7:edd6964c r6:00000001 r5:00000000
[ 10.329999] r4:00000000 r3:00000000
[ 10.333611] [<c00c291c>] (generic_file_read_iter) from [<c01e6958>] (nfs_file_read+0x54/0x8c)
[ 10.342168] r10:ebd23948 r9:ed2bc919 r8:00000080 r7:ecefdd98 r6:ecefdd0c r5:edd69570
[ 10.350072] r4:ecefdd20
[ 10.352628] [<c01e6904>] (nfs_file_read) from [<c0104b34>] (__vfs_read+0xb0/0xd8)
[ 10.360140] r6:ed1b2780 r5:00000000 r4:00000000 r3:c01e6904
[ 10.365858] [<c0104a84>] (__vfs_read) from [<c01051cc>] (vfs_read+0x84/0x108)
[ 10.373021] r8:c08136cc r7:ed1b2780 r6:ecefdd98 r5:ed733600 r4:ed1b2780
[ 10.379793] [<c0105148>] (vfs_read) from [<c0109d20>] (kernel_read+0x3c/0x54)
[ 10.386956] r9:ed2bc919 r8:c08136cc r7:ed1b2780 r6:00000000 r5:ed733600 r4:bf000000
[ 10.394780] [<c0109ce4>] (kernel_read) from [<c01489a0>] (load_elf_binary+0x1a0/0xfd0)
[ 10.402728] r4:ec93b600
[ 10.405281] [<c0148800>] (load_elf_binary) from [<c010ab04>] (search_binary_handler+0x7c/0x1c4)
[ 10.414014] r10:ebd23948 r9:c08136cc r8:c08136cc r7:00000001 r6:fffffff8 r5:c0813bc4
[ 10.421914] r4:ed733600
[ 10.424466] [<c010aa88>] (search_binary_handler) from [<c0148388>] (load_script+0x1fc/0x20c)
[ 10.432937] r9:c08136cc r8:c08136cc r7:00000001 r6:fffffff8 r5:00000000 r4:ed733600
[ 10.440757] [<c014818c>] (load_script) from [<c010ab04>] (search_binary_handler+0x7c/0x1c4)
[ 10.449141] r5:c0813ba8 r4:ed733600
[ 10.452749] [<c010aa88>] (search_binary_handler) from [<c010b2f8>] (do_execveat_common+0x40c/0x5b8)
[ 10.461832] r9:ec9db500 r8:000001da r7:ebd19000 r6:00000000 r5:ecef3700 r4:ed733600
[ 10.469650] [<c010aeec>] (do_execveat_common) from [<c010b4d8>] (do_execve+0x34/0x3c)
[ 10.477510] r10:00000000 r9:ecefc000 r8:c000f204 r7:0000000b r6:00000005 r5:be8563e8
[ 10.485411] r4:0003f7e0
[ 10.487962] [<c010b4a4>] (do_execve) from [<c010b728>] (SyS_execve+0x24/0x28)
[ 10.495132] [<c010b704>] (SyS_execve) from [<c000f060>] (ret_fast_syscall+0x0/0x3c)
[ 10.502818] r5:ffffffff r4:00027008
[ 10.506425] Code: e1a01006 eb07a8e1 e250c000 0a00001b (e59c4000)
[ 10.513054] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 10.538186] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 10.582154] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 10.594401] ---[ end trace fc3abe8a439e5d5f ]---
[ 10.602494] BUG: Bad rss-counter state mm:ecb12700 idx:1 val:2
[ 10.602632] scsi host0: ahci
[ 10.603033] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 353
[ 10.603289] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 10.603346] remoteproc1: 55020000.ipu is available
[ 10.603350] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 10.603352] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.603598] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
[ 10.603632] remoteproc2: 40800000.dsp is available
[ 10.603635] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 10.603638] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.604033] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[ 10.604070] remoteproc3: 41000000.dsp is available
[ 10.604073] remoteproc3: Note: remoteproc is still under development and considered experimental.
[ 10.604076] remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.608547] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 10.612833] remoteproc1: Direct firmware load for dra7-ipu2-fw.xem4 failed with error -2
[ 10.612835] remoteproc1: Falling back to user helper
[ 10.613672] remoteproc2: Direct firmware load for dra7-dsp1-fw.xe66 failed with error -2
[ 10.613675] remoteproc2: Falling back to user helper
[ 10.614357] remoteproc3: Direct firmware load for dra7-dsp2-fw.xe66 failed with error -2
[ 10.614359] remoteproc3: Falling back to user helper
[ 10.619373] vpe 489d0000.vpe: Direct firmware load for vpdma-1b8.bin failed with error -2
[ 10.619376] vpe 489d0000.vpe: Falling back to user helper
[ 10.665087] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
[ 10.672057] vpe 489d0000.vpe: couldn't get firmware
[ 10.789939] tmp102 0-0048: initialized
[ 10.791313] rtc-ds1307 2-006f: rtc core: registered mcp7941x as rtc0
[ 10.804842] rtc-ds1307 2-006f: 64 bytes nvram
[ 10.806430] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp/i2c@48070000/tlv320aic3104@18[0]'
[ 10.806558] aic_dvdd_fixed: supplied by vdd_3v3
[ 10.826756] remoteproc0: failed to load dra7-ipu1-fw.xem4
[ 10.832369] remoteproc3: failed to load dra7-dsp2-fw.xe66
[ 10.842622] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-gpio' property of node '/sound@0[0]'
[ 10.863363] palmas-rtc 48070000.i2c:tps659038@58:tps659038_rtc: rtc core: registered 48070000.i2c:tps659 as rtc1
[ 10.876287] remoteproc1: failed to load dra7-ipu2-fw.xem4
[ 10.889238] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-gpio' property of node '/sound@0[0]'
[ 10.902392] remoteproc2: failed to load dra7-dsp1-fw.xe66
[ 10.909280] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: GPIO lookup for consumer id
[ 10.931150] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using device tree for GPIO lookup
[ 10.947865] ata1: SATA link down (SStatus 0 SControl 300)
[ 10.947920] asoc-simple-card sound@0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 10.957815] of_get_named_gpiod_flags: parsed 'id-gpios' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]' - status (0)
[ 10.957823] no flags found for id
[ 10.988932] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: USB-HOST cable is detached
[ 11.004822] palmas_pwrbutton 48070000.i2c:tps659038@58:tps659038_pwr_button: h/w controlled shutdown duration=12 seconds
[ 11.030761] input: palmas_pwron as /devices/platform/44000000.ocp/48070000.i2c/i2c-0/0-0058/48070000.i2c:tps659038@58:tps659038_pwr_button/input/input0
[ 11.735611] usbcore: registered new interface driver usbfs
[ 11.741548] usbcore: registered new interface driver hub
[ 11.747282] usbcore: registered new device driver usb
[ 11.853046] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 11.858606] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 11.866655] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00010010
[ 11.875456] xhci-hcd xhci-hcd.1.auto: irq 443, io mem 0x48890000
[ 11.881654] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 11.888518] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 11.895771] usb usb1: Product: xHCI Host Controller
[ 11.900685] usb usb1: Manufacturer: Linux 4.1.6-g52c4aa7 xhci-hcd
[ 11.906802] usb usb1: SerialNumber: xhci-hcd.1.auto
[ 11.912462] hub 1-0:1.0: USB hub found
[ 11.916253] hub 1-0:1.0: 1 port detected
[ 11.920549] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 11.926065] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 11.933840] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 11.942090] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 11.948926] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 11.956190] usb usb2: Product: xHCI Host Controller
[ 11.961104] usb usb2: Manufacturer: Linux 4.1.6-g52c4aa7 xhci-hcd
[ 11.967222] usb usb2: SerialNumber: xhci-hcd.1.auto
[ 11.972846] hub 2-0:1.0: USB hub found
[ 11.976636] hub 2-0:1.0: 1 port detected
Please press Enter to activate this console. [ 12.237901] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 12.297811] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd
[ 12.318050] usb 2-1: New USB device found, idVendor=0451, idProduct=8140
[ 12.324802] usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 12.351117] hub 2-1:1.0: USB hub found
[ 12.355346] hub 2-1:1.0: 4 ports detected
[ 12.378077] usb 1-1: New USB device found, idVendor=0451, idProduct=8142
[ 12.384831] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[ 12.392051] usb 1-1: SerialNumber: CF010079C017
[ 12.415128] hub 1-1:1.0: USB hub found
[ 12.419072] hub 1-1:1.0: 4 ports detected
process '-/bin/sh' (pid 630) exited. Scheduling for restart.
Please press Enter to activate this console.
starting pid 634, tty '/dev/ttyS2': '-/bin/sh'
BusyBox v1.20.2 (2016-02-04 15:50:54 CST) built-in shell (ash)
Enter 'help' for a list of built-in commands.
/ #