Hi,
We are trying to bring up LCD on our custom board with DM6446, So have diagnostics code for programming LCD.
We have disabled PWM0,PW1 and PWM2 functionality in Pinmux1 register by modifing GEL file and RGB666 is enabled in PINMUX0.
but still if we probe on R2 and B2 line they are not toggling they still high.Do we need to do any other settings to make it functional?
One more problem is that we are not able to configure any GPIO line as output and drive low or high through that line with CCS and u-boot.
where are in linux it is working fine, GPIO module is enabled and MUX functionality is diapbled for the particular GPIO and DIR register of particular GPIO we are setting 0 to configure as o/p. but if we read back the value we are getting as 1 only.GPIO line is remaining high.
Please let us know if any additional settings need to be done in the s/w to make this work.
Thanks and Regards
Deepthi Kiran