Hi there,
i am using the Beaglebone Black with a 10.1'' 1280x800 Display.
When i play a video or so i am getting a message on the UART :
tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000020): FIFO underfow
And the Display looks like is ajusting it self or going on and off very fast.
On a reboot or when the system boot up i get this message:
of_graph_get_next_endpoint(): no port node found in /ocp/lcdc@4830e000
I think the DDR rate is too slow?
Any idea?