Is the 32 bit and 64 bit fixed point number format in Excess-32 or Two complement: with 31st bit signed and 30....0 bits magnitude?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the 32 bit and 64 bit fixed point number format in Excess-32 or Two complement: with 31st bit signed and 30....0 bits magnitude?
Hi Sherry,
[quote user="Sherry says"] Is the 32 bit and 64 bit fixed point number format in Excess-32 or Two complement: with 31st bit signed and 30....0 bits magnitude? [/quote ]
Please visit : 
Hi Shankari
This document does not tell about fixed point handling of C67x. it only tabulates SP and DP floating point handling with 24 bit mantissa and 8 bit exponent.