This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with tms320c5535 ezdsp

Hello,I'm having trouble with a device I bought from TI,the tmsc5535 ezdsp (for audio applications),the device works well when I run the test file in the attached disk (which includes required software and code composer studio),when I make this test routine,I can hear the audio file from the output of the device.

The problem is, I downloaded the teaching ROM from the TI web, and I followed meticoullously step by step the instructions in the power point examples,and the first program (the one that includes connecting a microphone and headphones) doesn't work,I can't hear anything from the output of the device,I tried with many different combinations of microphones and headphones,and I still can't hear anything.

The teaching ROM always mention the c5505 and c5515 ezdsp's devices,and all the configurations of the examples on it have only those two,I want to know if there's anything I have to change in the source files of Code Composer to make my c5535 work without problem.