This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LTE Library's DFT code output not matching with MATLAB DFT output



Hi All,

I'm using 6678 and LTE Library "ltelib_3_01_00_09_light". I'm trying to give a specific input to the DFT library and compare its output with that of MATLAB but it is not matching. Has any one else faced this issue..? Could any one get this working..?

I'm using 600 point DFT. I have used the test code provided in the example project for DFT as it is except that I'm feeding my own input to DFT code through some file IO. I have verified that that the input is copied to the ref_in buffer properly. But the output at the bufout buffer do not match with that of MATLAB output for the same input.

Regards,

Ashok