Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi,
In my custom board I have Redpine RS9113 WLAN/BT/ZB -module connected to USB0.
Linux used is mcsdk_1_01_00_02 linux-3.3-psp03.22.00.06.sdk, file system is based on tisdk-rootfs-image-omapl138-lcdk.tar.gz
I found thread:
https://e2e.ti.com/support/wireless_connectivity/wilink_wifi_bluetooth/f/307/p/35423/708113#708113
Which forwarded to wikis:
2) processors.wiki.ti.com/.../OMAP_WLAN_build_instructions_on_any_SDK
I've successfully compiled and installed rs9113 -related SW to Ubuntu (12.04) after loading libnl. Redpine instructions say about Makefile tuning: "The DEF_KERNEL_DIR variable has to be assigned the path of the compiled kernel path. For an x86 based Linux platform, this path is usually “/lib/modules/<kernel_version>/build” and this is the path assigned in the Makefile provided in the package".
DEF_KERNEL_DIR := /lib/modules/3.13.0-32-generic/build works for Ubuntu.
So I would like to ask:
1) Are wikis 1 and 2 valid for OMAP-L138 and mcsdk?
2) In Wiki 2 you recommend " Please, consult release notes for the board you are working with where the kernel patches can be downloaded" - could you forward me to source to download ones for l138 LCDK -compatible HW.
3) Where should this DEF_KERNEL_DIR point when cross-compiling?
4) Any easier methods to realize this all?
risto