Hi All,
I have some questions and some facts about McBSP and McSPI Clocks.
1. Besides using the same clock source (PER_96M_FCLK) McBSP2 and McBSP3 Clocks (CLKX) are not fully synchronized (Same Clock Phase).
2. The same way, McSPI3 clock is not synchronized with McBSP2/3 (All ports configured with same clock rate and to use clocks that came from 96M_FCLK).
3. By using the same clock source (96M_FCLK) shouldn't they be all synchronized? I mean, a little delay between then it's OK, but they start completely different each time I run my code.
I was wondering to use these ports in a device that has only a clock master, and all its communications interfaces has no clock input/output (they use Master Clock as reference).
So I need all clock fully synched. There is any way to do that?
Any help would be appreciated.
Thanks,
Danilo M. Caravana