Other Parts Discussed in Thread: ADS1262
Hello,
I am communicating with ADS1262 device via SPI using the following settings:
spiParams.frameFormat = SPI_POL0_PHA1;
I would like to add another spi device to my system: 
If I understand the datasheet, this device has different frameFormat settings:
spiParams.frameFormat = SPI_POL0_PHA0;
I would like to use the same SPI task for both device communication. Is it possible to update/change the frameFormat settings after SPI_open() ? Or I need to close and reopen SPI session with different frameformat settings?
Here is my SPI_Task fx:
/// --------------------------------------------------------------------------
/// SPICommunication handler Task
void SPICOMM_Task()
{
SPI_Handle spiHandle;
SPI_Params spiParams;
SPI_Transaction spiTransaction;
SPI_Params_init(&spiParams);
spiParams.frameFormat = SPI_POL0_PHA1;
spiParams.transferMode = SPI_MODE_BLOCKING;
spiParams.transferCallbackFxn = NULL;
spiHandle = SPI_open(Board_SPI0, &spiParams);
if (spiHandle == NULL)
{
System_abort("Error initializing SPI\n");
System_flush();
}
SPICOMM_QueueElement_t qelem, *qelemPtr;
qelemPtr = &qelem;
while(1)
{
Semaphore_pend(SPICOMM_Semaphore_Request,BIOS_WAIT_FOREVER);
qelemPtr = Queue_get(SPICOMM_Queue);
spiTransaction.txBuf = qelemPtr->writeBuffer; //(Ptr)request.writeBuffer;
spiTransaction.rxBuf = qelemPtr->readBuffer; //(Ptr)request.readBuffer;
spiTransaction.count = qelemPtr->count; //request.count;
GPIO_write(qelemPtr->SPI_CS,false);
if(!(SPI_transfer(spiHandle,&spiTransaction)))
{
GPIO_write(Board_LED1,true);
System_printf("SPI Bus Write Failed!\r\n");
System_flush();
}
GPIO_write(qelemPtr->SPI_CS,true);
if(qelemPtr->isWaitForResponse)
Semaphore_post(SPICOMM_Semaphore_Response);
}
}