I can't find the EDMA3 events mapping table.
It seems that the spruh79a doesn't illustrate the EDMA3 events mapping table.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thanks for your post.
Each DMA channel and QDMA channel can be independently programmed to map to a specific queue using
the DMA queue number register n (DMAQNUMn) and the QDMA channel queue number register
(QDMANUM) and the mapping of DMA/QDMA channels is critical to achieving the desired performance level for the EDMA. For more insight, please refer section 16.2.10 in TRM
For Event, Channel, and PaRAM Mapping, kindly refer section 16.2.6 in the TRM below:
http://www.ti.com/lit/ug/spruh79a/spruh79a.pdf
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------