This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Leopard LI-3M01 HD Camera with 6446 DVEVM error no libposixtime.o.1 module



When  compiling  the Leopard ver. 1.30 preview routines I receive the compiler error can't find command -lposixtime, indicating that the posixtime library was not found.  I can not find it anywhere.  Is it not shipped with the montavista pro500 that comes with the DVEVM dvsdk 2_00_00_22 that is available from the Ti site.  When attempting to run the precompiled previews they respond with can't load shared library libposixtime.so.1  which is most likely the same problem.

Any suggestions?