This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Leopard LI-3M01 HD Camera Board with Davinci 6446 DVEVM ---ERROR cant find libposixtime.so.1

I am trying to bring up the leopard camera on the 6446 DVEVM with dvsdk_2_00_00_22.  I have no trouble installing their suggested patches and re-building the kernel; however, when I try to compile the Leopard preview examples fro their version 1.30 package I receive the make error can't find command -lposixtime indicating that the posixtime library is not present.  I can't find it anywhere; it was not in the Ti download package which contains the Montavista Pro 500 Linux.  In addition when I try to run the Leopard precompiled preview examples, they fail and respond can't load shared library libposixtime.so.1 which is probably the same problem, they aren't there.  Does anyone have experience with this camera board with the DVEVM or know where to find the library?

Any other suggestions?