This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with codec's sample client application



Hi,

i'm trying to get running a sample client application, included in mpeg4enc distribution. It is compiled w/o any warnings or errors but hangs in PROCESS call. C64+ simulator, C6748 based silicon, both have same problem. Different versions of the framework, dsp/bios and code geenration tools doesn't help.

Compilation was done according to SPRAP73.

SW versions:

Encoder : 2.2.4

Bios: 5.31.08

FC: 2.20.1

CG: 6.0.8

 

Any idead?

 

  • Hello.
    I have the same problem. The algorithm does not return from the function process.
    retVal = ividEncfxns-> process ((IVIDENC1_Handle) handle,
    (IVIDEO1_BufDescIn *) & inputBufDesc,
    (XDM_BufDesc *) & outputBufDesc,
    (IVIDENC1_InArgs *) & inArgs,
    (IVIDENC1_OutArgs *) & outArgs_ext);

    omap33 you solved the problem?

    Malyshev

  • Hello,

    no, we couldnt solve this issue.

    It seems that TI just ignore this thread and is not interrested in cutsomer support. I tried already to contact TI stuff member, who published IMAP-L138 MPEG4 performance, but never received a responce from her.

    Any way its a GOOD example how UNIMPORTANT is a cutomer support for TI. :-(

  • There are similar themes! I give the link to the topic of this codec can find the answer, I have not found (

    http://e2e.ti.com/support/embedded/f/356/p/52531/246311.aspx # 246311