In Silicon Errata (SPRZ429H), i880 describes that RGMII2 is limited to 10/100 Mbps. For SR 2.0, IO timing characterization is pending.
For SR 2.0, are RGMII2 Switching Characteristics not compatible with 1000 Mbps operation?
Here is the performance information for Ethernet Port0: http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Kernel_Performance_Guide
It will show the performance when only RGMII1 is used.
Please tell me the performance when only RGMII2 is used and when ports of both RGMII1 and RGMII2 are used.
Best regards,
Daisuke