This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

does DM6446 support DDR2-800(200Mhz)???

Hi,

Is DM6446 has support for DDR2-800(i.e. 200 Mhz, 256MB)??

DM6446 DDR controller can support DDR speed only upto 166 Mhz and that using a higher speed DDR will limit the speed to the maximum supported speed of 166 Mhz.

If the above assumption is correct, please suggest what all changes required in the boot loader to change the DDR2 speed.

Thanks!!!

regards

Sathish