Other Parts Discussed in Thread: OMAPL138
Previous Post: e2e.ti.com/.../1765623
Right now I am trying to use Timer Interrupt to switch on/off GPIO. Here is part of the code:
/* Start the timer. */ TimerEnable(SOC_TMR_2_REGS, TMR_TIMER12, TMR_ENABLE_CONT);
/*
** Setup the timer for 64 bit mode
*/
static void TimerSetUp64Bit(void)
{
/* Configuration of Timer */
TimerConfigure(SOC_TMR_2_REGS, TMR_CFG_64BIT_CLK_INT);
/* Set the 64 bit timer period */
TimerPeriodSet(SOC_TMR_2_REGS, TMR_TIMER12, TMR_PERIOD_LSB32);
TimerPeriodSet(SOC_TMR_2_REGS, TMR_TIMER34, TMR_PERIOD_MSB32);
}
However, ~52kHz seems to be the upper limit for the timer interrupt and I cannot increase it further when I reduce TMR_PERIOD_LSB32. As I am looking to have an interrupt at ~MHz range, is there anything I can change to achieve that?
Also, I have a difficult time to look up for the base frequency of the Timer. What section/page of the Manual I should look into?
Thank you.