Other Parts Discussed in Thread: AM3352
Hi
We are using two SPI port in AM3352. We are using pins B13(SPI1_D0), D12(SPI1_D1), C12(SPI1_CS0), A13(SPI0_SCLK) and B17(SPI0_D0), B16(SPI0_D1), A16(SPI0_CS0), A17(SPI0_SCLK) for SPI1 and SPI0 port. In TRM it is mentioned that SPI0 is used for boot EEPROM. Please let us know if we can used two different SPI port as assigned above separately and access simultaneously.
Both SPI should be configured as Master.
Regards
Manoj A