This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

evm oob no ip address

Hello All,

I am a complete newbie at this, trying to move from matlab to real-time DSP, so please excuse any shortcomings of the following post.

I followed the TMDSEVM6657LS quick setup guide and can communicate with the board over USB but cannot get IP address.  The boot successfully got through these steps:

IBL version: 1.0.0.15
IBL: Booting from NOR
platform_init Done
Start BIOS 6
HUA version 2.00.00.04
Setting hostname to tidemo-237397
MAC Address: 00-18-30-03-2B-CB
Configuring DHCP client

as indicated in the quick setup guide. Now it continues to cycle on the following four responses:

Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000

and never gives me an IP address, as shown in the setup guide.

I am using Windows 7 64-bit. I have turned off the Windows firewall, am using OfficeScan Agent anti-virus.  I have cycled the power on the board, restarted Windows, hit the reset button on the board multiple times. I have searched through e2e and google and found nothing that can help.  Hoping this direct method helps.

Thanks,

Bill