This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM57x: Slow memory access of shared memory



Hi,

We have observed that both read and write access to shared memory is costly both in terms of time and CPU usage. We have seen this issue in two scenarios

1. We have some data on the shared buffer, we are trying to parse this buffer to perform some operations. We see that this operation takes around 21ms and 50% of the CPU. Where as if we were to memcopy the shared buffer to a linux buffer, and do the same parsing, it takes around 2ms and 2-3% of the CPU.

2. When we use shared memory buffer for the h264 decoder (our own decoder running on ARM) output, we see that the decode time is around 150ms. Where as if linux buffers are used for decoder output, we see that it operates at sub 16ms range. 

This looks like some cashing issue. Can you please help us understand why is this difference seen? 

Regards,

Apoorva

  • Hi,

    I will ask the video experts to comment.
  • Hi Apoorva,

     

    Where are you getting the shared memory from?

    1. If you are getting omap GEM buffer (omapdrm and IVA) then it uses TILER memory.

    2. FYI, V4L2 memory is from CMA and is DMA memory.

       

    Both these memories are write-combine cache type. Write-combine memory behaves as no cache for reading and costly for non-sequential write operations. Sequential writes performance should be comparable to cached memory. In addition, the TILER memory paging has additional overhead for setup/teardown steps, so that causes some overhead when taking a buffer into use or freeing it.

     

    For non-sequential writes and/or read type operations, below two suggestion for generic processing of video buffers on ARM or DSP for broader customer use cases -

    1.  Allocate the buffers using omap_bo_new() with flags set to OMAP_BO_CACHED. When caching is used, the user must handle cache flushing and cache coherency when applicable.

      1. If V4l2, allocate the buffer using omap_bo_new and export them using V4L2_MEMORY_DMABUF option.

         

    2. Let CPU operate on local buffers and not directly access the video buffers. Use DMA and ping-pong mechanism to transfer the data in small chunks from/to video buffers to local memory (L2/L1 for DSP). Process the data from the local memory in small chunks and hide the dma overhead through ping-pong mechanism in processing background.

    Regards,

    Manisha

        

  • Hi,

    We are trying to allocate buffers using omap_bo_new() with flags set to OMAP_BO_CACHED.
    These buffers are used for the output of VPE (resized output), we update these buffers to overlay some information using memset() and provide it to encoder.
    The encoded data has problem with the parts which has been updated post VPE.

    I think this is seen as we are not taking care of cache flushing and cache coherency.
    Please let us know how to handle cache flushing and cache coherency?

    It would be helpful if you can point to any existing implementation.

    Thank you in advance.

    Regards,
    Krishna
  • Hi,

    We are making omap_bo_cpu_prep call before updating buffers and omap_bo_cpu_fini call after updating buffers.
    The updated part of video has issues even after making these calls.

    Regards,
    Krishna
  • Krishna,

    OMAP_BO_CACHED feature is broken in the driver.

    Mainline has added DMA_BUF_IOCTL_SYNC ioctl for managing cached dmabufs. We are exploring this API to enable dmabuf cache management once cache handling gets fixed inside driver. Do not have time line to commit anything but we are looking to enable cache management of dmabufs.

    Regards,

    Manisha

  • Hi Manisha,

    Any chance we have or will have it fixed soon?

    Regards, Oleg
  • Hi Oleg,

    This has been taken care in PSDK 3.2 using CMEM buffers. The CMEM driver already had support for cached buffers and now they are enhanced to support dambuf export feature. So for scenarios where CPU need to access buffers, we recommend those buffers to be allocated using CMEM and then exported to the drivers with which they need to be shared. Example can be found in dual camera demo example source code in PSDK.
  • Thank you for reply.
    I see only PSDK 3.01 available. Where dual-camera example uses omap_drm APIs.
    Is there any way to make it work on PSDK 3.01? Or way to get 3.2 soon?
  • Oleg,

    PSDK 3.2 is already available. I see the dual camera demo example application in PSDK 3.2 is not updated to demonstrate CMEM API usage. Find attached source file for loopback.c with CMEM API usage. 

    #include <stdlib.h>
    #include <unistd.h>
    #include <errno.h>
    #include <string.h>
    #include <fcntl.h>
    #include <sys/mman.h>
    #include <malloc.h>
    #include <sys/stat.h>
    #include <sys/ioctl.h>
    #include <stdbool.h>
    #include <linux/videodev2.h>
    #include <linux/dma-buf.h>
    #include <omap_drm.h>
    #include <omap_drmif.h>
    #include <xf86drmMode.h>
    #include "jpeg.h"
    #include "loopback.h"
    
    #define USE_CMEM_BUF
    #define PROFILE_ENABLE
    #define CMEM_BLOCKID CMEM_CMABLOCKID
    //#define USE_DMABUF_MMAP
    
    #ifdef PROFILE_ENABLE
    #include <time.h>
    #define CACHED_BUFFERS
    #define CACHE_SIZE 0x200000
    #define MAX_PROFILE_POINTS 100
    #define DISP_POINTS_PER_ROW 4
    #endif
    
    #ifdef USE_CMEM_BUF
    #include <ti/cmem.h>
    #endif
    
    #define ERROR(fmt, ...) \
    	do { fprintf(stderr, "ERROR:%s:%d: " fmt "\n", __func__, __LINE__,\
    ##__VA_ARGS__); } while (0)
    
    #define MSG(fmt, ...) \
    	do { fprintf(stderr, fmt "\n", ##__VA_ARGS__); } while (0)
    
    /* Dynamic debug. */
    #define DBG(fmt, ...) \
    	do { fprintf(stderr, fmt "\n", ##__VA_ARGS__); } while (0)
    
    /* align x to next highest multiple of 2^n */
    #define ALIGN2(x,n)   (((x) + ((1 << (n)) - 1)) & ~((1 << (n)) - 1))
    #define FOURCC(a, b, c, d) ((uint32_t)(uint8_t)(a) | \
    	((uint32_t)(uint8_t)(b) << 8) | ((uint32_t)(uint8_t)(c) << 16) | \
    	((uint32_t)(uint8_t)(d) << 24 ))
    #define FOURCC_STR(str)    FOURCC(str[0], str[1], str[2], str[3])
    
    #define PAGE_SHIFT 12
    #define NBUF (3)
    #define MAX_DRM_PLANES 5
    #define CAP_WIDTH 800
    #define CAP_HEIGHT 600
    #define PIP_POS_X  25
    #define PIP_POS_Y  25
    #define MAX_ZORDER_VAL 3 //For AM57x device, max zoder value is 3
    
    struct control status;
    
    struct dmabuf_buffer {
    	uint32_t fourcc, width, height;
    	int nbo;
    #ifdef USE_CMEM_BUF
    	void *cmem_buf[4];
    #endif
    	struct omap_bo *bo[4];
    	uint32_t pitches[4];
    	int fd[4];		/* dmabuf */
    	unsigned fb_id;
    };
    
    struct connector_info {
    	unsigned int id;
    	char mode_str[64];
    	drmModeModeInfo *mode;
    	drmModeEncoder *encoder;
    	int crtc;
    	int pipe;
    };
    
    /*
    * drm output device structure declaration
    */
    struct drm_device_info
    {
    	int fd;
    	int width;
    	int height;
    	char dev_name[9];
    	char name[4];
    	unsigned int bo_flags;
    	struct dmabuf_buffer **buf[2];
    	struct omap_device *dev;
    	unsigned int crtc_id;
    	unsigned int plane_id[2];
    	unsigned int prop_fbid;
    	unsigned int prop_crtcid;
    	uint64_t zorder_val_primary_plane;
    	uint64_t trans_key_mode_val;
    	uint32_t zorder_val[MAX_DRM_PLANES-1];
    } drm_device;
    
    /*
    * V4L2 capture device structure declaration
    */
    struct v4l2_device_info {
    	int type;
    	int fd;
    	enum v4l2_memory memory_mode;
    	unsigned int num_buffers;
    	int width;
    	int height;
    	char dev_name[12];
    	char name[10];
    
    	struct v4l2_buffer *buf;
    	struct v4l2_format fmt;
    	struct dmabuf_buffer **buffers;
    } cap0_device, cap1_device;
    #ifdef PROFILE_ENABLE
    #define MAX_FRAME_SIZE 0x100000
    int process_frame_cnt=0;
    static uint32_t process_time_cnt, inv_time_cnt, wb_time_cnt;
    static uint32_t process_time_array[MAX_PROFILE_POINTS];
    static uint32_t avg_process_time=0, min_process_time=0xffffffff, max_process_time=0;
    static uint32_t avg_inv_time=0, min_inv_time=0xffffffff, max_inv_time=0;
    static uint32_t avg_wb_time=0, min_wb_time=0xffffffff, max_wb_time=0;
    /**
     *  @brief Function clock_diff returns difference between two timeval
     *  @param[in]     start            start time
     *  @param[in]     end              end time
     *  @retval        deltaTime
     */
    static int64_t clock_diff (struct timespec *start, struct timespec *end)
    {
        return (end->tv_sec - start->tv_sec) * 1000000000 
                 + end->tv_nsec - start->tv_nsec;
    }
    #endif
    
    #ifdef USE_CMEM_BUF
    int dma_buf_do_cache_operation(int dma_buf_fd, uint32_t cache_operation) {
    	int ret;
    	struct dma_buf_sync sync;
    	sync.flags = cache_operation;
    
    	ret = ioctl(dma_buf_fd, DMA_BUF_IOCTL_SYNC, &sync);
    
    	return ret;
    }
    
    CMEM_AllocParams cmem_alloc_params = {
    	CMEM_HEAP,	/* type */
    #ifdef CACHED_BUFFERS
    	CMEM_CACHED,	/* flags */
    #else
    	CMEM_NONCACHED,	/* flags */
    #endif
    	1		/* alignment */
    };
    
    static void *alloc_cmem_buffer(unsigned int size, unsigned int align)
    {
    	void *cmem_buf;
    
    	cmem_alloc_params.alignment = align;
    	
    	DBG("\n allocating cmem buffer of size 0x%x", size);
    
    	cmem_buf = CMEM_alloc2(CMEM_BLOCKID, size,
    		&cmem_alloc_params);
    	return cmem_buf ;
    }
    
    static void free_cmem_buffer(void *cmem_buffer)
    {
    
    	CMEM_free(cmem_buffer,
    		&cmem_alloc_params);
    }
    
    static struct omap_bo *alloc_omap_bo_with_cmembuf(struct drm_device_info *device,
    		unsigned int bpp,
    		unsigned int width, unsigned int height,
    		unsigned int *bo_handle, unsigned int *pitch,
    		void **cmem_buf, int *dma_buf_fd)
    {
    	unsigned int bo_flags = device->bo_flags;
    	int ret;
    	int size;
    	struct omap_bo *bo;
    
    	size = (width*height*bpp/8);
    
    	/* Allocate CMEM buffer */
    	/* TODO: Add any alignment requirements here */
    	*cmem_buf = alloc_cmem_buffer(size, 1);
    	if ( *cmem_buf == NULL ) {
    		return NULL;
    	}
    
    	/* Export cmem buf as dma buf */
    	*dma_buf_fd = CMEM_export_dmabuf(*cmem_buf);
    	if ( *dma_buf_fd < 0 ) {
    		free_cmem_buffer(cmem_buf);
    		return NULL;
    	}
    
    	/* Get a bo_handle for the dma buffer */
    	ret = drmPrimeFDToHandle(device->fd, *dma_buf_fd, (uint32_t *)bo_handle);
    	if (ret) {
    		ERROR("drmPrimeFDToHandle failed: %s (%d)", strerror(errno), ret);
    		free_cmem_buffer(cmem_buf);
    		return NULL;
    	} else {
    		*pitch = width * bpp / 8;
    		if (bo_flags & OMAP_BO_TILED)
    			*pitch = ALIGN2(*pitch, PAGE_SHIFT);
    	}
    
    	/* Get the bo allocted by the previous step */
    	bo = omap_bo_from_dmabuf(device->dev, *dma_buf_fd);
    
    	return bo;
    }
    #else
    static struct omap_bo *alloc_bo(struct drm_device_info *device, unsigned int bpp,
    		unsigned int width, unsigned int height,
    		unsigned int *bo_handle, unsigned int *pitch)
    {
    	struct omap_bo *bo;
    	unsigned int bo_flags = device->bo_flags;
    
    	bo_flags |= OMAP_BO_WC;
    	bo = omap_bo_new(device->dev, width * height * bpp / 8, bo_flags);
    
    	if (bo) {
    		*bo_handle = omap_bo_handle(bo);
    		*pitch = width * bpp / 8;
    		if (bo_flags & OMAP_BO_TILED)
    			*pitch = ALIGN2(*pitch, PAGE_SHIFT);
    	}
    
    	return bo;
    }
    #endif
    #ifdef USE_DMABUF_MMAP
    void *cmem_dmabuf_map(int dma_buf_fd, int size)
    {
    	void *dmabuf_mmap;
    	int offset=0;
    #ifdef DEBUG
    	DBG("\n mmap called: dma_buf_fd %d, size %x \n", dma_buf_fd, size);
    #endif
    	dmabuf_mmap = mmap(0, size, PROT_READ | PROT_WRITE,
    			MAP_SHARED, dma_buf_fd, offset);
    
    	return dmabuf_mmap;
    }
    #endif
    //You can use DRM ioctl as well to allocate buffers (DRM_IOCTL_MODE_CREATE_DUMB)
    //and drmPrimeHandleToFD() to get the buffer descriptors
    static struct dmabuf_buffer *alloc_buffer(struct drm_device_info *device,
    		unsigned int fourcc, unsigned int w,
    		unsigned int h)
    {
    	struct dmabuf_buffer *buf;
    	unsigned int bo_handles[4] = {0}, offsets[4] = {0};
    	int ret;
    
    	buf = (struct dmabuf_buffer *) calloc(1, sizeof(struct dmabuf_buffer));
    	if (!buf) {
    		ERROR("allocation failed");
    		return NULL;
    	}
    
    	buf->fourcc = fourcc;
    	buf->width = w;
    	buf->height = h;
    	buf->nbo = 1;
    #ifdef USE_CMEM_BUF
    	buf->bo[0] = alloc_omap_bo_with_cmembuf(device, 16, buf->width, buf->height,
    		&bo_handles[0], &buf->pitches[0], &buf->cmem_buf[0], &buf->fd[0]);
    	if (buf->bo[0] == NULL) {
    		ERROR("alloc_omap_bo_with_cmembuf failed: %s", strerror(errno) );
    		return NULL;
    	}
    #else
    	buf->bo[0] = alloc_bo(device, 16, buf->width, buf->height,
    		&bo_handles[0], &buf->pitches[0]);
    #endif
    	ret = drmModeAddFB2(device->fd, buf->width, buf->height, fourcc,
    		bo_handles, buf->pitches, offsets, &buf->fb_id, 0);
    
    	if (ret) {
    		ERROR("drmModeAddFB2 failed: %s (%d)", strerror(errno), ret);
    		return NULL;
    	}
    
    	return buf;
    }
    
    void free_vid_buffers(struct dmabuf_buffer **buf, unsigned int n)
    {
    	unsigned int i;
    
    	if (buf == NULL) return;
    	for (i = 0; i < n; i++) {
    		if (buf[i]) {
    			close(buf[i]->fd[0]);
    			omap_bo_del(buf[i]->bo[0]);
    #ifdef USE_CMEM_BUF
    			free_cmem_buffer(buf[i]->cmem_buf[0]);
    #endif
    			free(buf[i]);
    		}
    	}
    	free(buf);
    }
    
    
    static struct dmabuf_buffer **get_vid_buffers(struct drm_device_info *device,
    		unsigned int n,
    		unsigned int fourcc, unsigned int w, unsigned int h)
    {
    	struct dmabuf_buffer **bufs;
    	unsigned int i = 0;
    
    	bufs = (struct dmabuf_buffer **) calloc(n, sizeof(*bufs));
    	if (!bufs) {
    		ERROR("allocation failed");
    		goto fail;
    	}
    
    	for (i = 0; i < n; i++) {
    		bufs[i] = alloc_buffer(device, fourcc, w, h);
    		if (!bufs[i]) {
    			ERROR("allocation failed");
    			goto fail;
    		}
    	}
    	return bufs;
    
    fail:
    	return NULL;
    }
    
    static int v4l2_init_device(struct v4l2_device_info *device)
    {
    	int ret;
    	struct v4l2_capability capability;
    
    	/* Open the capture device */
    	device->fd = open((const char *) device->dev_name, O_RDWR);
    	if (device->fd <= 0) {
    		printf("Cannot open %s device\n", device->dev_name);
    		return -1;
    	}
    
    	MSG("\n%s: Opened Channel\n", device->name);
    
    	/* Check if the device is capable of streaming */
    	if (ioctl(device->fd, VIDIOC_QUERYCAP, &capability) < 0) {
    		perror("VIDIOC_QUERYCAP");
    		goto ERROR;
    	}
    
    	if (capability.capabilities & V4L2_CAP_STREAMING)
    		MSG("%s: Capable of streaming\n", device->name);
    	else {
    		ERROR("%s: Not capable of streaming\n", device->name);
    		goto ERROR;
    	}
    
    	{
    		struct v4l2_streamparm streamparam;
    		streamparam.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    		if (ioctl(device->fd, VIDIOC_G_PARM, &streamparam) < 0){
    			perror("VIDIOC_G_PARM");
    			goto ERROR;
    		}
    	}
    
    	device->fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    	ret = ioctl(device->fd, VIDIOC_G_FMT, &device->fmt);
    	if (ret < 0) {
    		ERROR("VIDIOC_G_FMT failed: %s (%d)", strerror(errno), ret);
    		goto ERROR;
    	}
    
    	device->fmt.fmt.pix.pixelformat = FOURCC_STR("YUYV");
    	device->fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    	device->fmt.fmt.pix.width = device->width;
    	device->fmt.fmt.pix.height = device->height;
    
    	ret = ioctl(device->fd, VIDIOC_S_FMT, &device->fmt);
    	if (ret < 0) {
    		perror("VIDIOC_S_FMT");
    		goto ERROR;
    	}
    
    	MSG("%s: Init done successfully\n", device->name);
    	return 0;
    
    ERROR:
    	close(device->fd);
    
    	return -1;
    }
    
    static void v4l2_exit_device(struct v4l2_device_info *device)
    {
    
    	free(device->buf);
    	close(device->fd);
    
    	return;
    }
    
    
    /*
    * Enable streaming for V4L2 capture device
    */
    static int v4l2_stream_on(struct v4l2_device_info *device)
    {
    	enum v4l2_buf_type type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    	int ret = 0;
    
    	ret = ioctl(device->fd, VIDIOC_STREAMON, &type);
    
    	if (ret) {
    		ERROR("VIDIOC_STREAMON failed: %s (%d)", strerror(errno), ret);
    	}
    
    	return ret;
    }
    
    /*
    * Disable streaming for V4L2 capture device
    */
    static int v4l2_stream_off(struct v4l2_device_info *device)
    {
    	enum v4l2_buf_type type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    	int ret = -1;
    
    	if (device->fd <= 0) {
    		return ret;
    	}
    
    	ret = ioctl(device->fd, VIDIOC_STREAMOFF, &type);
    
    	if (ret) {
    		ERROR("VIDIOC_STREAMOFF failed: %s (%d)", strerror(errno), ret);
    	}
    
    	return ret;
    }
    
    static int v4l2_request_buffer(struct v4l2_device_info *device,
    		struct dmabuf_buffer **bufs)
    {
    	struct v4l2_requestbuffers reqbuf;
    	unsigned int i;
    	int ret,dmafd;
    
    	if (device->buf) {
    		// maybe eventually need to support this?
    		ERROR("already reqbuf'd");
    		return -1;
    	}
    
    	reqbuf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    	reqbuf.memory = device->memory_mode;
    	reqbuf.count = device->num_buffers;
    
    	ret = ioctl(device->fd, VIDIOC_REQBUFS, &reqbuf);
    	if (ret < 0) {
    		ERROR("VIDIOC_REQBUFS failed: %s (%d)", strerror(errno), ret);
    		return ret;
    	}
    
    	if ((reqbuf.count != device->num_buffers) ||
    		(reqbuf.type != V4L2_BUF_TYPE_VIDEO_CAPTURE) ||
    		(reqbuf.memory != V4L2_MEMORY_DMABUF)) {
    			ERROR("unsupported..");
    			return -1;
    	}
    
    	device->num_buffers = reqbuf.count;
    	device->buffers = bufs;
    	device->buf = (struct v4l2_buffer *) calloc(device->num_buffers, \
    			sizeof(struct v4l2_buffer));
    	if (!device->buf) {
    		ERROR("allocation failed");
    		return -1;
    	}
    
    	for (i = 0; i < device->num_buffers; i++) {
    		if (bufs[i]->nbo != 1){
    			ERROR("Number of buffers not right");
    		};
    
    #ifdef USE_CMEM_BUF
    		dmafd = bufs[i]->fd[0];
    #else
    		/* Call omap_bo_dmabuf only once, to export only once
    		* Otherwise, each call will return duplicated fds
    		* This way, every call to omap_bo_dmabuf will return a new fd
    		* Which won't match with any previously exported fds
    		* Instead, store dma fd in buf->fd[] */
    		dmafd = omap_bo_dmabuf(bufs[i]->bo[0]);
    		bufs[i]->fd[0] = dmafd;
    #endif
    		device->buf[i].type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    		device->buf[i].memory = V4L2_MEMORY_DMABUF;
    		device->buf[i].index = i;
    
    		MSG("Exported buffer fd = %d\n", dmafd);
    		ret = ioctl(device->fd, VIDIOC_QUERYBUF, &device->buf[i]);
    		device->buf[i].m.fd = dmafd;
    
    		if (ret) {
    			ERROR("VIDIOC_QUERYBUF failed: %s (%d)", strerror(errno), ret);
    			return ret;
    		}
    	}
    
    	return 0;
    }
    
    /*
    * Queue V4L2 buffer
    */
    static int v4l2_queue_buffer(struct v4l2_device_info *device,
    		struct dmabuf_buffer *buf)
    {
    	struct v4l2_buffer *v4l2buf = NULL;
    	int  ret, fd;
    	unsigned char i;
    
    	if(buf->nbo != 1){
    		ERROR("number of bufers not right\n");
    		return -1;
    	}
    
    	fd = buf->fd[0];
    
    	for (i = 0; i < device->num_buffers; i++) {
    		if (device->buf[i].m.fd == fd) {
    			v4l2buf = &device->buf[i];
    		}
    	}
    
    	if (!v4l2buf) {
    		ERROR("invalid buffer");
    		return -1;
    	}
    	ret = ioctl(device->fd, VIDIOC_QBUF, v4l2buf);
    	if (ret) {
    		ERROR("VIDIOC_QBUF failed: %s (%d)", strerror(errno), ret);
    	}
    
    	return ret;
    }
    
    /*
    * DeQueue V4L2 buffer
    */
    struct dmabuf_buffer *v4l2_dequeue_buffer(struct v4l2_device_info *device)
    {
    	struct dmabuf_buffer *buf;
    	struct v4l2_buffer v4l2buf;
    	int ret;
    
    	v4l2buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    	v4l2buf.memory = V4L2_MEMORY_DMABUF;
    	ret = ioctl(device->fd, VIDIOC_DQBUF, &v4l2buf);
    	if (ret) {
    		ERROR("VIDIOC_DQBUF failed: %s (%d)\n", strerror(errno), ret);
    		return NULL;
    	}
    
    	buf = device->buffers[v4l2buf.index];
    
    	device->buf[v4l2buf.index].timestamp = v4l2buf.timestamp;
    	if(buf->nbo != 1){
    		ERROR("num buffers not proper\n");
    		return NULL;
    	}
    
    	return buf;
    }
    
    
    
    unsigned int get_drm_prop_val(int fd, drmModeObjectPropertiesPtr props,
    							  const char *name)
    {
    	drmModePropertyPtr p;
    	unsigned int i, prop_id = 0; /* Property ID should always be > 0 */
    
    	for (i = 0; !prop_id && i < props->count_props; i++) {
    		p = drmModeGetProperty(fd, props->props[i]);
    		if (!strcmp(p->name, name)){
    			prop_id = p->prop_id;
    			break;
    		}
    		drmModeFreeProperty(p);
    	}
    	if (!prop_id) {
    		printf("Could not find %s property\n", name);
    		drmModeFreeObjectProperties(props);
    		exit(-1);
    	}
    
    	drmModeFreeProperty(p);
    	return props->prop_values[i];
    }
    
    unsigned int find_drm_prop_id(int fd, drmModeObjectPropertiesPtr props,
    							  const char *name)
    {
    	drmModePropertyPtr p;
    	unsigned int i, prop_id = 0; /* Property ID should always be > 0 */
    
    	for (i = 0; !prop_id && i < props->count_props; i++) {
    		p = drmModeGetProperty(fd, props->props[i]);
    		if (!strcmp(p->name, name)){
    			prop_id = p->prop_id;
    			break;
    		}
    		drmModeFreeProperty(p);
    	}
    	if (!prop_id) {
    		printf("Could not find %s property\n", name);
    		drmModeFreeObjectProperties(props);
    		exit(-1);
    	}
    
    	return prop_id;
    }
    
    void add_property(int fd, drmModeAtomicReqPtr req,
    				  drmModeObjectPropertiesPtr props,
    				  unsigned int plane_id,
    				  const char *name, int value)
    {
    	unsigned int prop_id = find_drm_prop_id(fd, props, name);
    
    //	DBG("\n add_property: fd %d, plane_id %d, name %s, value %d", fd, plane_id, name, value);
    
    	if(drmModeAtomicAddProperty(req, plane_id, prop_id, value) < 0){
    		printf("failed to add property\n");
    	}
    }
    
    void drm_add_plane_property(struct drm_device_info *dev, drmModeAtomicReqPtr req)
    {
    	unsigned int i;
    	unsigned int crtc_x_val = 0;
    	unsigned int crtc_y_val = 0;
    	unsigned int crtc_w_val = dev->width;
    	unsigned int crtc_h_val = dev->height;
    	drmModeObjectProperties *props;
    	unsigned int zorder_val = 1;
    	unsigned int buf_index;
    	struct v4l2_device_info  *v4l2_device;
    
    	for(i = 0; i < status.num_cams; i++){
    		unsigned int plane_id = dev->plane_id[i];
    
    		if(i) {
    			crtc_x_val = PIP_POS_X;
    			crtc_y_val = PIP_POS_Y;
    			crtc_w_val /= 3;
    			crtc_h_val /= 3;
    		}
    		props = drmModeObjectGetProperties(dev->fd, plane_id,
    			DRM_MODE_OBJECT_PLANE);
    
    		if(props == NULL){
    			ERROR("drm obeject properties for plane type is NULL\n");
    			exit (-1);
    		}
    
    		//fb id value will be set every time new frame is to be displayed
    		dev->prop_fbid = find_drm_prop_id(drm_device.fd, props, "FB_ID");
    
    		//Will need to change run time crtc id to disable/enable display of plane
    		dev->prop_crtcid = find_drm_prop_id(drm_device.fd, props, "CRTC_ID");
    
    		//storing zorder val to restore it before quitting the demo
    		drm_device.zorder_val[i] = get_drm_prop_val(drm_device.fd, props, "zorder");
    
    		//Set the fb id based on which camera is chosen to be main camera 
    		if (status.main_cam  == 1){
    			buf_index = (i+1)%2;
    		}
    		else {
    			buf_index = i;
    		}
    
    		if(buf_index == 0){
    			v4l2_device = &cap0_device;
    		}
    		else{
    			v4l2_device = &cap1_device;
    		}
    		printf("w=%d, h=%d\n", v4l2_device->width, v4l2_device->height);
    		add_property(dev->fd, req, props, plane_id, "FB_ID", dev->buf[buf_index][0]->fb_id);
    
    		//set the plane properties once. No need to set these values every time
    		//with the display of frame. 
    		add_property(dev->fd, req, props, plane_id, "CRTC_ID", dev->crtc_id);
    		add_property(dev->fd, req, props, plane_id, "CRTC_X", crtc_x_val);
    		add_property(dev->fd, req, props, plane_id, "CRTC_Y", crtc_y_val);
    		add_property(dev->fd, req, props, plane_id, "CRTC_W", crtc_w_val);
    		add_property(dev->fd, req, props, plane_id, "CRTC_H", crtc_h_val);
    		add_property(dev->fd, req, props, plane_id, "SRC_X", 0);
    		add_property(dev->fd, req, props, plane_id, "SRC_Y", 0);
    		add_property(dev->fd, req, props, plane_id, "SRC_W", v4l2_device->width << 16);
    		add_property(dev->fd, req, props, plane_id, "SRC_H", v4l2_device->height << 16);
    		add_property(dev->fd, req, props, plane_id, "zorder", zorder_val++);
    	}
    }
    
    uint32_t drm_reserve_plane(int fd, unsigned int *ptr_plane_id, int num_planes)
    {
    	unsigned int i;
    	int idx = 0;
    	drmModeObjectProperties *props;
    	drmModePlaneRes *res = drmModeGetPlaneResources(fd);
    	if(res == NULL){
    		ERROR("plane resources not found\n");
    	}
    
    	for (i = 0; i < res->count_planes; i++) {
    		uint32_t plane_id = res->planes[i];
    		unsigned int type_val;
    
    		drmModePlane *plane = drmModeGetPlane(fd, plane_id);
    		if(plane == NULL){
    			ERROR("plane  not found\n");
    		}
    
    		props = drmModeObjectGetProperties(fd, plane->plane_id, DRM_MODE_OBJECT_PLANE);
    
    		if(props == NULL){
    			ERROR("plane (%d) properties not found\n",  plane->plane_id);
    		}
    
    		type_val = get_drm_prop_val(fd, props, "type");
    
    		if(type_val == DRM_PLANE_TYPE_OVERLAY){
    			ptr_plane_id[idx++] = plane_id;
    		}
    
    		drmModeFreeObjectProperties(props);
    		drmModeFreePlane(plane);
    
    		if(idx == num_planes){
    			drmModeFreePlaneResources(res);
    			return 0;
    		}
    	}
    
    	ERROR("plane couldn't be reserved\n");
    	return -1;
    }
    
    
    /* Get crtc id and resolution. */
    void drm_crtc_resolution(struct drm_device_info *device)
    {
    	drmModeCrtc *crtc;
    	int i;
    
    	drmModeResPtr res = drmModeGetResources(device->fd);
    
    	if (res == NULL){
    		ERROR("drmModeGetResources failed: %s\n", strerror(errno));
    		exit(0);
    	};
    
    	for (i = 0; i < res->count_crtcs; i++) {
    		unsigned int crtc_id = res->crtcs[i];
    
    		crtc = drmModeGetCrtc(device->fd, crtc_id);
    		if (!crtc) {
    			DBG("could not get crtc %i: %s\n", res->crtcs[i], strerror(errno));
    			continue;
    		}
    		if (!crtc->mode_valid) {
    			drmModeFreeCrtc(crtc);
    			continue;
    		}
    
    		printf("CRTCs size: %dx%d\n", crtc->width, crtc->height);
    		device->crtc_id = crtc_id;
    		device->width = crtc->width;
    		device->height = crtc->height;
    
    		drmModeFreeCrtc(crtc);
    	}
    
    	drmModeFreeResources(res);
    }
    
    /*
    * DRM restore properties
    */
    static void drm_restore_props(struct drm_device_info *device)
    {
    	unsigned int i;
    	drmModeObjectProperties *props;
    	int ret;
    
    	drmModeAtomicReqPtr req = drmModeAtomicAlloc();
    
    	props = drmModeObjectGetProperties(device->fd, device->crtc_id,
    		DRM_MODE_OBJECT_CRTC);
    
    	//restore trans-key-mode and z-order of promary plane
    	add_property(device->fd, req, props, device->crtc_id, "trans-key-mode", \
    			device->trans_key_mode_val);
    	add_property(device->fd, req, props, device->crtc_id, "zorder", \
    			device->zorder_val_primary_plane);
    
    	//restore z-order of overlay planes
    	for(i = 0; i < status.num_cams; i++){
    		props = drmModeObjectGetProperties(device->fd, device->plane_id[i],
    			DRM_MODE_OBJECT_PLANE);
    
    		if(props == NULL){
    			ERROR("drm obeject properties for plane type is NULL\n");
    			exit (-1);
    		}
    
    		add_property(device->fd, req, props, device->plane_id[i], \
    				"zorder", device->zorder_val[i]);
    	}
    
    	//Commit all the added properties
    	ret = drmModeAtomicCommit(device->fd, req, DRM_MODE_ATOMIC_TEST_ONLY, 0);
    	if(!ret){
    		drmModeAtomicCommit(device->fd, req, 0, 0);
    	}
    	else{
    		ERROR("ret from drmModeAtomicCommit = %d\n", ret);
    	}
    
    	drmModeAtomicFree(req);
    }
    
    /*
    * drm device init
    */
    static int drm_init_device(struct drm_device_info *device)
    {
    	if (!device->fd) {
    		device->fd = drmOpen("omapdrm", NULL);
    		if (device->fd < 0) {
    			ERROR("could not open drm device: %s (%d)", strerror(errno), errno);
    			return -1;
    		}
    	}
    
    	drmSetClientCap(device->fd, DRM_CLIENT_CAP_UNIVERSAL_PLANES, 1);
    	drmSetClientCap(device->fd, DRM_CLIENT_CAP_ATOMIC, 1);
    
    	device->dev = omap_device_new(device->fd);
    
    	/* Get CRTC id and resolution. As well set the global display width and height */
    	drm_crtc_resolution(device);
    
    	/* Store display resolution so GUI can be configured */
    	status.display_xres = device->width;
    	status.display_yres = device->height;
    
    	drm_reserve_plane(device->fd, device->plane_id, status.num_cams);
    
    	return 0;
    }
    
    /*
    *Clean resources while exiting drm device
    */
    static void drm_exit_device(struct drm_device_info *device)
    {
    	drm_restore_props(device);
    	drmSetClientCap(device->fd, DRM_CLIENT_CAP_UNIVERSAL_PLANES, 0);
    	drmSetClientCap(device->fd, DRM_CLIENT_CAP_ATOMIC, 0);
    
    	omap_device_del(device->dev);
    	device->dev = NULL;
    	if (device->fd > 0) {
    		close(device->fd);
    	}
    
    	return;
    }
    
    /*
    * Set up the DSS for blending of video and graphics planes
    */
    static int drm_init_dss(void)
    {
    	drmModeObjectProperties *props;
    	int ret;
        FILE *fp;
        char str[10];
        char trans_key_mode = 2;
    
    	/*
    	* Dual camera demo is supported on Am437x and AM57xx evm. Find which
    	* specific SoC the demo is running to set the trans key mode -
    	* found at the corresponding TRM, for example,
    	* For AM437x: trans_key_mode = 1 GFX Dest Trans
    	*             TransKey applies to GFX overlay, marking which
    	*              pixels come from VID overlays)
    	* For AM57xx: trans_key_mode = 2 Source Key.
    	*             Match on Layer4 makes Layer4 transparent (zorder 3)
    	*
    	* The deault mode is 1 for backward compatibility
    	*/
    
    	fp = fopen("/proc/sys/kernel/hostname", "r");
    	fscanf(fp, "%s", str);
    
    	//terminate the string after the processor name. "-evm" extension is
    	//ignored in case the demo gets supported on other boards like idk etc
    	str[6] = '\0';
    	printf("Running the demo on %s processor\n", str);
    
    	//Set trans-key-mode to 1 if dual camera demo is running on AM437x
    	if (strcmp(str,"am437x") == 0){
    		trans_key_mode = 1;
    	}
    
    	drmModeAtomicReqPtr req = drmModeAtomicAlloc();
    
    	/* Set CRTC properties */
    	props = drmModeObjectGetProperties(drm_device.fd, drm_device.crtc_id,
    		DRM_MODE_OBJECT_CRTC);
    
    	drm_device.zorder_val_primary_plane = get_drm_prop_val(drm_device.fd,
    		props, "zorder");
    	drm_device.trans_key_mode_val = get_drm_prop_val(drm_device.fd, props,
    		"trans-key-mode");
    
    	add_property(drm_device.fd, req, props, drm_device.crtc_id,
    		"trans-key-mode", trans_key_mode);
    	add_property(drm_device.fd, req, props, drm_device.crtc_id,
    		"alpha_blender", 1);
    	add_property(drm_device.fd, req, props, drm_device.crtc_id,
    		"zorder", MAX_ZORDER_VAL);
    
    	/* Set overlay plane properties like zorder, crtc_id, buf_id, src and */
    	/* dst w, h etc                                                       */
    	drm_add_plane_property(&drm_device, req);
    
    	//Commit all the added properties
    	ret = drmModeAtomicCommit(drm_device.fd, req, DRM_MODE_ATOMIC_TEST_ONLY, 0);
    
    //	DBG("\ndrm_init_dss: drmModeAtomicCommit done, ret %d\n",ret);;fflush(stdout);
    
    	if(!ret){
    		drmModeAtomicCommit(drm_device.fd, req, 0, 0);
    	}
    	else{
    		ERROR("ret from drmModeAtomicCommit = %d\n", ret);
    		return -1;
    	}
    
    	drmModeAtomicFree(req);
    	return 0;
    }
    
    
    /*
    * drm disable pip layer
    */
    void drm_disable_pip(void)
    {
    	int ret;
    	drmModeAtomicReqPtr req = drmModeAtomicAlloc();
    
    	drmModeAtomicAddProperty(req, drm_device.plane_id[1],
    		drm_device.prop_fbid, 0);
    	drmModeAtomicAddProperty(req, drm_device.plane_id[1],
    		drm_device.prop_crtcid, 0);
    
    	ret = drmModeAtomicCommit(drm_device.fd, req,
    		DRM_MODE_ATOMIC_TEST_ONLY, 0);
    	if(!ret){
    		drmModeAtomicCommit(drm_device.fd, req,
    			0, 0);
    	}
    	else{
    		ERROR("failed to enable plane %d atomically: %s",
    			drm_device.plane_id[!status.main_cam], strerror(errno));
    	}
    
    	drmModeAtomicFree(req);
    }
    
    void drm_enable_pip(void)
    {
    	int ret;
    
    	drmModeAtomicReqPtr req = drmModeAtomicAlloc();
    
    	drmModeAtomicAddProperty(req, drm_device.plane_id[1],
    		drm_device.prop_fbid, drm_device.buf[!status.main_cam][0]->fb_id);
    	drmModeAtomicAddProperty(req, drm_device.plane_id[1],
    		drm_device.prop_crtcid, drm_device.crtc_id);
    
    	ret = drmModeAtomicCommit(drm_device.fd, req,
    		DRM_MODE_ATOMIC_TEST_ONLY, 0);
    
    	if(!ret){
    		drmModeAtomicCommit(drm_device.fd, req, 0, 0);
    	}
    	else{
    		ERROR("failed to enable plane %d atomically: %s",
    			drm_device.plane_id[!status.main_cam], strerror(errno));
    	}
    
    	drmModeAtomicFree(req);
    }
    
    /*
    * Capture v4l2 frame and save to jpeg
    */
    static int capture_frame(struct v4l2_device_info *v4l2_device,
    						 struct dmabuf_buffer *buf)
    {
    
    	jpegWrite(omap_bo_map(buf->bo[0]),
    		status.num_jpeg, v4l2_device->width, v4l2_device->height);
    
    	return 0;
    }
    
    /*
    * Initialize the app resources with default parameters
    */
    void default_parameters(void)
    {
    	/* Main camera display */
    	memset(&drm_device, 0, sizeof(drm_device));
    	strcpy(drm_device.dev_name,"/dev/drm");
    	strcpy(drm_device.name,"drm");
    	drm_device.width=0;
    	drm_device.height=0;
    	drm_device.bo_flags = OMAP_BO_SCANOUT;
    	drm_device.fd = 0;
    
    	/* Main camera */
    	cap0_device.memory_mode = V4L2_MEMORY_DMABUF;
    	cap0_device.num_buffers = NBUF;
    	strcpy(cap0_device.dev_name,"/dev/video1");
    	strcpy(cap0_device.name,"Capture 0");
    	cap0_device.buffers = NULL;
    	cap0_device.fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_YUYV;
    	cap0_device.width = CAP_WIDTH;
    	cap0_device.height = CAP_HEIGHT;
    
    	/* PiP camera */
    	cap1_device.memory_mode = V4L2_MEMORY_DMABUF;
    	cap1_device.num_buffers = NBUF;
    	strcpy(cap1_device.dev_name,"/dev/video0");
    	strcpy(cap1_device.name,"Capture 1");
    	cap1_device.buffers = NULL;
    	cap1_device.fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_YUYV;
    	cap1_device.width = CAP_WIDTH;
    	cap1_device.height = CAP_HEIGHT;
    
    	/* Set the default parameters for device options */
    	status.main_cam=0;
    	status.num_cams=2;
    	status.num_jpeg=0;
    	if(status.num_cams == 1){
    		status.pip=false;
    	}
    	else{
    		status.pip=true;
    	}
    	status.jpeg=false;
    	status.exit=false;
    
    	/* Ensure that jpeg image save directory exists */
    	mkdir("/usr/share/camera-images/", 0777);
    
    	return;
    }
    
    /*
    * Free resource and exit devices
    */
    void exit_devices(void)
    {
    	v4l2_exit_device(&cap0_device);
    	if (status.num_cams==2) {
    		v4l2_exit_device(&cap1_device);
    	}
    	free_vid_buffers(drm_device.buf[0], NBUF);
    	free_vid_buffers(drm_device.buf[1], NBUF);
    	drm_exit_device(&drm_device);
    }
    
    /*
    * End camera streaming
    */
    void end_streaming(void)
    {
    	v4l2_stream_off(&cap0_device);
    	if (status.num_cams==2) {
    		v4l2_stream_off(&cap1_device);
    	}
    }
    
    void set_plane_properties()
    {
    	int ret;
    	drmModeAtomicReqPtr req = drmModeAtomicAlloc();
    
    	req = drmModeAtomicAlloc();
    
    	drmModeAtomicAddProperty(req, drm_device.plane_id[0],
    		drm_device.prop_fbid, drm_device.buf[status.main_cam][0]->fb_id);
    
    	if(status.pip){
    		drmModeAtomicAddProperty(req, drm_device.plane_id[1],
    			drm_device.prop_fbid, drm_device.buf[!status.main_cam][0]->fb_id);
    	}
    	ret = drmModeAtomicCommit(drm_device.fd, req,
    		DRM_MODE_ATOMIC_TEST_ONLY, 0);
    	if(!ret){
    		drmModeAtomicCommit(drm_device.fd, req,
    			0, 0);
    	}
    	else{
    		ERROR("failed to enable plane %d atomically: %s",
    			drm_device.plane_id[!status.main_cam], strerror(errno));
    	}
    	drmModeAtomicFree(req);
    }
    /*
    * Initializes all drm and v4l2 devices for loopback
    */
    int init_loopback(void)
    {
    	bool status_cam0 = 0;
    	bool status_cam1 = 0;
    
    	/* Declare properties for video and capture devices */
    	default_parameters();
    
    
    #ifdef USE_CMEM_BUF
    	CMEM_init();
    #endif
    	/* Initialize the drm display devic */
    	if (drm_init_device(&drm_device)) goto Error;
    
    	/* Check to see if the display resolution is very small.  If so, the
    	* camera capture resolution needs to be lowered so that the scaling
    	* limits of the DSS are not reached */
    	if (drm_device.width < 640) {
    		/* Set capture 0 device resolution */
    		cap0_device.width = 640;
    		cap0_device.height = 480;
    
    		/* Set capture 1 device resolution */
    		cap1_device.width = 640;
    		cap1_device.height = 480;
    	}
    
    	/* Initialize the v4l2 capture devices */
    	if (v4l2_init_device(&cap0_device) < 0) {
    		printf("first camera detection failed\n");
    		/* If there is not a second camera, program can still continue */
    		status.num_cams=1;
    		status.main_cam=1;
    		status.pip=false;
    	}
    	else{
    		unsigned int i;
    		struct dmabuf_buffer **buffers = get_vid_buffers(&drm_device, cap0_device.num_buffers, 
    			cap0_device.fmt.fmt.pix.pixelformat, cap0_device.width, cap0_device.height);
    
    		if (!buffers) {
    			goto Error;
    		}
    
    		drm_device.buf[0] = buffers;
    
    		/* Pass these buffers to the capture drivers */
    		if (v4l2_request_buffer(&cap0_device, buffers) < 0) {
    			goto Error;
    		}
    
    		for (i = 0; i < cap0_device.num_buffers; i++) {
    			v4l2_queue_buffer(&cap0_device, buffers[i]);
    		}
    
    		status_cam0 = 1;
    	}
    
    	if(v4l2_init_device(&cap1_device) < 0) {
    		/* If there is not a second camera, program can still continue */
    		if(status.num_cams ==2){
    			status.num_cams=1;
    			status.pip=false;
    			printf("Only one camera detected\n");
    		}
    		//first camera wasn't detected
    		else if (!status_cam0){
    			printf("No camera detected\n");
    			goto Error;
    		}
    	}
    	else{
    		unsigned int i;
    		struct dmabuf_buffer **buffers = get_vid_buffers(&drm_device, cap1_device.num_buffers, 
    			cap1_device.fmt.fmt.pix.pixelformat, cap1_device.width, cap1_device.height);
    		if (!buffers) {
    			goto Error;
    		}
    
    		drm_device.buf[1] = buffers;
    
    		/* Pass these buffers to the capture drivers */
    		if (v4l2_request_buffer(&cap1_device, buffers) < 0) {
    			goto Error;
    		}
    
    		for (i = 0; i < cap1_device.num_buffers; i++) {
    			v4l2_queue_buffer(&cap1_device, buffers[i]);
    		}
    
    		status_cam1 = 1;
    	}
    
    	/* Enable streaming for the v4l2 capture devices */
    	if(status_cam0){
    		if (v4l2_stream_on(&cap0_device) < 0) goto Error;
    	}
    
    	if (status_cam1) {
    		if (v4l2_stream_on(&cap1_device) < 0) goto Error;
    	}
    
    	/* Configure the DSS to blend video and graphics layers */
    	if (drm_init_dss() < 0 ) goto Error;
    
    	return 0;
    
    Error:
    	status.exit = true;
    	return -1;
    }
    
    static void page_flip_handler(int fd, unsigned int frame,
    							  unsigned int sec, unsigned int usec,
    							  void *data)
    {
    	int *waiting_for_flip = data;
    	*waiting_for_flip = 0;
    }
    
    /*
    * Determines which camera feeds are being displayed and
    * whether a jpeg image needs to be captured.
    */
    void process_frame(void)
    {
    	fd_set fds;
    	int ret, waiting_for_flip = 1;
    	struct dmabuf_buffer *buf[2] = {NULL, NULL};
    	drmModeAtomicReqPtr req = drmModeAtomicAlloc();
    
    	struct v4l2_device_info *v4l2_device[2] =
    	{&cap0_device, &cap1_device};
    	int i, j;
    	volatile uint32_t *buffer_pointer;
    	
    #ifdef PROFILE_ENABLE
    	int size, remaining_size, transfer_size, block_size_in_words;
    	struct timespec tp_start, tp_inv_finish, tp_operation, tp_end;
    #endif
    
    	drmEventContext evctx = {
    		.version = DRM_EVENT_CONTEXT_VERSION,
    		.vblank_handler = 0,
    		.page_flip_handler = page_flip_handler,
    	};
    
    	/* Request a capture buffer from the driver that can be copied to */
    	/* framebuffer */
    	buf[status.main_cam] =
    		v4l2_dequeue_buffer(v4l2_device[status.main_cam]);
    
    #ifdef PROFILE_ENABLE
    	size = (buf[status.main_cam]->width*buf[status.main_cam]->height*16/8);
    	block_size_in_words = CACHE_SIZE/(sizeof(uint32_t));
    
    	clock_gettime(CLOCK_MONOTONIC, &tp_start);
    #ifdef USE_CMEM_BUF
    #ifdef CACHED_BUFFERS
    	/* Add code to invalidate cache */
    	dma_buf_do_cache_operation(buf[status.main_cam]->fd[0], (DMA_BUF_SYNC_START | DMA_BUF_SYNC_READ));
    #endif
    #endif
    
    	clock_gettime(CLOCK_MONOTONIC, &tp_inv_finish);
    #ifdef USE_CMEM_BUF
    #ifdef USE_DMABUF_MMAP
    	buffer_pointer = (volatile uint32_t *)(cmem_dmabuf_map(buf[status.main_cam]->fd[0], size));
    	if (buffer_pointer == MAP_FAILED) {
    		ERROR("\n Error mmap with dmabuf_fd, error: %s\n", strerror(errno));fflush(stdout);
    		return;	
    	}
    #else
    	buffer_pointer = (volatile uint32_t *)(buf[status.main_cam]->cmem_buf[0]);
    #endif
    #else
    	buffer_pointer = (volatile uint32_t *)(omap_bo_map(buf[status.main_cam]->bo[0]));
    #endif
    	/* Do operations on the buffer: Currently doing dummy add and subtract 1 */
    	remaining_size=size;
    	i = 0;
    	do {
    		transfer_size = (remaining_size > CACHE_SIZE) ? CACHE_SIZE : remaining_size;
    		for (j=0; j < (transfer_size/(int)sizeof(uint32_t)); j++) {
    			buffer_pointer[(i*block_size_in_words)+j] = buffer_pointer[(i*block_size_in_words)+j]+1;
    		}
    		for (j=0; j < (transfer_size/(int)sizeof(uint32_t)); j++)
    			buffer_pointer[(i*block_size_in_words)+j] = buffer_pointer[(i*block_size_in_words)+j]-1;
    		i++;
    		remaining_size -= transfer_size;
    	} while( remaining_size > 0);
    
    	clock_gettime(CLOCK_MONOTONIC, &tp_operation);
    #ifdef USE_CMEM_BUF
    #ifdef CACHED_BUFFERS
    	/* Add code to writeback cache */
    	dma_buf_do_cache_operation(buf[status.main_cam]->fd[0], (DMA_BUF_SYNC_WRITE |DMA_BUF_SYNC_END));
    #endif
    
    #ifdef USE_DMABUF_MMAP
    	munmap((void *)buffer_pointer, size);
    #endif
    #endif
    	clock_gettime(CLOCK_MONOTONIC, &tp_end);
    
    	/* Calculate time deltas and min , max values */
    	process_time_cnt = clock_diff (&tp_start, &tp_end);
    	avg_process_time = (avg_process_time + process_time_cnt )/2;
    	min_process_time = (process_time_cnt < min_process_time) ? process_time_cnt : min_process_time;
    	max_process_time = (process_time_cnt > max_process_time) ? process_time_cnt : max_process_time;
    	inv_time_cnt = clock_diff (&tp_start, &tp_inv_finish);
    	avg_inv_time = (avg_inv_time + inv_time_cnt )/2;
    	min_inv_time = (inv_time_cnt < min_inv_time) ? inv_time_cnt : min_inv_time;
    	max_inv_time = (inv_time_cnt > max_inv_time) ? inv_time_cnt : max_inv_time;
    	wb_time_cnt = clock_diff (&tp_operation, &tp_end);
    	avg_wb_time = (avg_wb_time + wb_time_cnt )/2;
    	min_wb_time = (avg_wb_time < min_wb_time) ? avg_wb_time : min_wb_time;
    	max_wb_time = (avg_wb_time > max_wb_time) ? avg_wb_time : max_wb_time;
    	if ((process_frame_cnt >= 0) && (process_frame_cnt < MAX_PROFILE_POINTS))
    		process_time_array[process_frame_cnt] = process_time_cnt;
    		
    	if(process_frame_cnt == MAX_PROFILE_POINTS) {
    		int k, l;
    		printf("\n avg_process_time %d ns, min_process_time %d ns, max_process_time %d ns\n",
    			avg_process_time, min_process_time, max_process_time);
    		printf("\n avg_inv_time %d ns, min_inv_time %d ns, max_inv_time %d ns\n",
    			avg_inv_time, min_inv_time, max_inv_time);
    		printf("\n avg_wb_time %d ns, min_wb_time %d ns, max_wb_time %d ns\n",
    			avg_wb_time, min_wb_time, max_wb_time);
    		for(k=0; k< MAX_PROFILE_POINTS/DISP_POINTS_PER_ROW; k++) {
    			printf("\n");
    			for ( l=0; l< DISP_POINTS_PER_ROW; l++)
    				printf("%d ", process_time_array[(DISP_POINTS_PER_ROW*k)+l]);
    		}
    	}
    	process_frame_cnt++;
    #endif
    	drmModeAtomicAddProperty(req, drm_device.plane_id[0],
    		drm_device.prop_fbid, buf[status.main_cam]->fb_id);
    
    //	DBG("\n process_frame: drmModeAtomicAddProperty complete prop_fbid %d fb_id %d",
    //		drm_device.prop_fbid , buf[status.main_cam]->fb_id);
    
    	if (status.pip==true) {
    		buf[!status.main_cam] =
    			v4l2_dequeue_buffer(v4l2_device[!status.main_cam]);
    		drmModeAtomicAddProperty(req, drm_device.plane_id[1],
    			drm_device.prop_fbid, buf[!status.main_cam]->fb_id);
    	}
    
    	ret = drmModeAtomicCommit(drm_device.fd, req,
    		DRM_MODE_ATOMIC_TEST_ONLY, 0);
    
    //	DBG("\n process_frame: drmModeAtomicCommit, ret %d", ret);
    
    	if(!ret){
    		drmModeAtomicCommit(drm_device.fd, req,
    			DRM_MODE_PAGE_FLIP_EVENT | DRM_MODE_ATOMIC_NONBLOCK, &waiting_for_flip);
    		}
    		else {
    		ERROR("failed to add plane atomically: %s", strerror(errno));
    		}
    
    	drmModeAtomicFree(req);
    
    	/* Save jpeg image if triggered */
    	if (status.jpeg==true) {
    		capture_frame(v4l2_device[status.main_cam], buf[status.main_cam]);
    		status.jpeg=false;
    		status.num_jpeg++;
    		if (status.num_jpeg==10)
    			status.num_jpeg=0;
    	}
    
    	FD_ZERO(&fds);
    	FD_SET(drm_device.fd, &fds);
    
    	while (waiting_for_flip) {
    		ret = select(drm_device.fd + 1, &fds, NULL, NULL, NULL);
    		if (ret < 0) {
    			printf("select err: %s\n", strerror(errno));
    			return;
    		}
    		else if (ret == 0) {
    			printf("select timeout!\n");
    			return;
    		}
    		else if (FD_ISSET(0, &fds)) {
    			continue;
    		}
    		drmHandleEvent(drm_device.fd, &evctx);
    	}
    
    	v4l2_queue_buffer(v4l2_device[status.main_cam], buf[status.main_cam]);
    	if(status.pip == true){
    		v4l2_queue_buffer(v4l2_device[!status.main_cam], buf[!status.main_cam]);
    	}
    }
    

    Regards,

    Manisha

  • Hmm, Was I blind or 3.02 just popped up on TI's web.

    Thank you very much. Let me try to cmem now.

    Updsate: Hmm, quite painfull to try

    1. CMEM in PSDK 3.2 has only  0x100000 bytes but I cannot allocate them.

    test tool for CMEM: "apitest 16"

    just fails from beginning:

    root@am57xx-evm:~/tmp/edma-mngr-test# apitest 128
    CMEM initialized.
    CMEM version = 0x4120000
    testMap: ptr = 0xaaea3000
    writing 0xdadaface to *ptr
    testMap: remapped physp 0xa0000000 to 0xb6fc7000
    *map_ptr = 0xdadaface
    testMap: original pointer still good
    testMap: trying to map too much (0x800)...
    testMap: CMEM_map() should've failed but didn't
    testAllocPhys: mapped physp 0xa0000000 to 0xb6fc7000 785.481666] cmem cmem: coherent DMA mask is unset

    writing 0xdadaface to *map_ptr
    *map_ptr = 0xdadaface
    unmapping 0xb6fc7000
    testAllocPhys: trying to map too much (0x800)...
    testAllocPhys: CMEM_map() should've failed but didn't
    allocating heap buffers from CMA memory block...
    (will end with expected failed allocation)
    785.512571] CMEMK Error: ioctl: failed to allocate heap buffer of size 0x1000
    MECM Error: allocHeap: ioctl CMEM_IOCALLOCHEAP failed: -1
    ...don, 0 allocated
    Press ENTER to continue

    2. Tried to use one BIG (190MB) CMEM pool, available there, but discovered it is used by OpenCL (it is used even even if __malloc_ddr is not called) 

    3. CMEM_export_dmabuf(...) is not part of cmem library in PSDK 3.02