Hello,
We designed a new board with AM3352 having a eMMC chip on MMC1 (pin-mux mode 2).
But we did not design the pullups on the eMMC lines, thinking the internal PU will be Ok.
Now we got the boards and have troubles, the bus is not running in 8 or 4 data width mode, only the mode 1 bit is working.
We rechecked the pin-muxing, measured the data-lines connection and layout, and everythink seems to be ok.
We aslo tried to reduce the clock, but behavior is the same. U-boot SW seems also to work properly. The SD Card on MMC0 works with 4 data bits, but here we have the pullups...
So can be the mssing external pullups on the reason?
Thanks
Jean-Luc