This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt in AM335x based beagleboard black not getting set



Hi,

Thank you for your time.

I have added utils, drive, platform and systems

I cannot get the interrupts going for Timer (or uart).

On further investigation i found that the timer module is working just fine and is giving a overflow status.

The issue is with CPSR resistor in the core.

I am unable to enable interrupts by resetting the IRQ bit in the CPSR resistor.

Where R0 = 0x40000110

CPSR = 0x40000190

When i do a  msr     CPSR, r0

I still get CPSR = 0x40000190

IRQ is disabled... 

I am sure that I am missing something here,.. can anyone please help

Code below for reference -

#include "dmtimer.h"
#include "interrupt.h"
#include "gpio_v2.h"

#include "soc_AM335x.h"
#include "beaglebone.h"

static void hardware_init();
static void timer_init();
static void timer_config(unsigned long, unsigned long);
static void isr_timer2();

int main(void) {
// Set up hardware and peripherals.
hardware_init();

// Configure timer settings
timer_config(0xF0000000u, 0xF0000000u);
timer_init();


// XXX: Turn on LED
GPIOPinWrite(SOC_GPIO_1_REGS, (23), GPIO_PIN_HIGH);

// Enable timer interrupt
DMTimerIntEnable(SOC_DMTIMER_2_REGS, DMTIMER_INT_OVF_EN_FLAG);

// Turn on actual timer
DMTimerEnable(SOC_DMTIMER_2_REGS);

asm(" mrs r0, CPSR");
asm(" bic r0, r0, #0x80");
asm(" msr CPSR, r0");

// Loop forever- all work takes place in ISRs.
while(1);
}


static void hardware_init() {
// Configure GPIO/LED
GPIO1ModuleClkConfig();
GPIO1Pin23PinMuxSetup();
GPIOModuleEnable(SOC_GPIO_1_REGS);
GPIOModuleReset(SOC_GPIO_1_REGS);

/* Set GPIO 1.23 as output */
GPIODirModeSet(SOC_GPIO_1_REGS, (23), GPIO_DIR_OUTPUT);
}

static void timer_init() {
// Set up the configuration for the hardware timer.

/* Enable clocks for DMTimer2 */
DMTimer2ModuleClkConfig();

/* Initialize ARM interrupt controller (AINTC) */
IntAINTCInit();

/* Register our ISR to DMTimer2's interrupt. */
IntRegister(SYS_INT_TINT2, isr_timer2);

/* Set the DMTimer2's interrupt priority to 0. */
IntPrioritySet(SYS_INT_TINT2, 0, AINTC_HOSTINT_ROUTE_IRQ);

/* Enable the DMTimer2 interrupt. */
IntSystemEnable(SYS_INT_TINT2);

/* Enable IRQ in CPSR (ARM program status register) */
// IntMasterIRQEnable();

}

static void timer_config(unsigned long initial, unsigned long reload) {
// Configure timer
// Note that instead of doing a count from 0 to some compare value, we are
// preloading the timer with a given value and watching for it to overflow,
// which is functionally identical.

/* Configure the timer mode. */
// Modes: autoreload (selected) versus one-shot mode. Does the timer automatically reset itself?
// compare versus overflow (selected) mode. Does the timer ISR trip on equality to a value, or on overflow?
DMTimerModeConfigure(SOC_DMTIMER_2_REGS, DMTIMER_AUTORLD_NOCMP_ENABLE);

/* Load initial counter value into timer. */
DMTimerCounterSet(SOC_DMTIMER_2_REGS, initial);

/* Load reload counter value into timer, the value the timer gets every time it is reset. */
DMTimerReloadSet(SOC_DMTIMER_2_REGS, reload);
}

// Interrupt vector for BeagleBone timer
static void isr_timer2() {
static short int mode = 0;

/* Disable the DMTimer interrupt */
DMTimerIntDisable(SOC_DMTIMER_2_REGS, DMTIMER_INT_OVF_EN_FLAG);

/* Clear the interrupt flags (IF) status */
DMTimerIntStatusClear(SOC_DMTIMER_2_REGS, DMTIMER_INT_OVF_IT_FLAG);

/* *********** ISR TASKS BEGIN *********** */
if (mode == 0) {
// Turn on LED
GPIOPinWrite(SOC_GPIO_1_REGS, (23), GPIO_PIN_HIGH);
mode = 1;
} else {
// Turn off LED
GPIOPinWrite(SOC_GPIO_1_REGS, (23), GPIO_PIN_LOW);
mode = 0;
}
/* *********** ISR TASKS END *********** */

/* Re-enable the DMTimer interrupt */
DMTimerIntEnable(SOC_DMTIMER_2_REGS, DMTIMER_INT_OVF_EN_FLAG);
}

IRQ CPSR.doc