Other Parts Discussed in Thread: AM3359
Can anyone explain while following the CCS instructions to build and run the i2c_led example I would get the following error after doing "Build project" step:
error: cannot find file "rtsv7A8_A_le_n_v3_eabi.lib"
* The GEL file is loaded fine
* Debug Connected to the AM3359 just fine
Looks like the compile is ok - there is just an issue with the linker.
File search on the computer finds:
"rtsv7A8_T_le_n_v3_eabi.lib" in ..\ccsv6\tools\compiler\ti-cgt-arm_5.2.7\lib
so I am guessing in that using the "Refactor" command to update both the RTSC and compiler I messed up something.