This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can DM8127 be replaced by DM8148 ?



Hi all:

The board is designed for DM8127 and it functions well (with DVRRDK-04.XXXXXX)

What if DM8148 is soldered on the board designed for DM8127 ???????

Does the board still work fine ????

Notes:

The board is adapted from IPNC-camera design and TPS659113 is used to power the DM8127

DVRRDK 4.xxxx is used instead of IPNC-RDK (as we don't use the cameraLink, we need the captureLink)