Hi,
I am new to this LCD interface but would appreciate if someone can help me understand what types of LCD interface (in terms of user connector pins) can AM1808 processor connect to? I am not talking about the board connector on the experimental board, which uses 60 pins connectors. What I am talking about is the internal user interface pins defined by LCD manufacturer (such as 40pins, 45pins or 54pins depends on manufacturer... For instance, the experimental board uses Sharp LCD which uses 40 pins internally.)
I read some wiki answer on this topic and found a LCD controller which gives more details ("SPRUFM0A" doc). In particular the LIDD controller which defines how AM1808's LCD controller can be compatible with different other types of displays. However, it's not so clear to me how those pins can be mapped accordingly for different types of LCD? For instance, what type of display is the one that currently connected to experimental board? 6800 family or 8080 family??
Please advise.
Thanks