Other Parts Discussed in Thread: OMAPL138
Everyone:
I use the RTFS system to read and write SATA on the OMAP-L138 board. And I use bios_5_41_13_42, rtfs_1_10_02_32, pspdrivers_01_30_01.
When I do the ATA_DrvInit() , I stucked in the ATA_SubmitIdentify() function:
pReq -> Retry = 10u;
ATA_SubmitReq (pDevice, pReq);
while (pReq -> Retry != 0)
{
//PAL_osWaitMsecs (1u);
m_delay(1u);
//pReq -> Retry--;
}
I find other codes alike in the ata.c, as following:
static Int32 ATA_MaxLba (ATA_Drive_t *pDevice)
{
ATA_Dev_Req_t *pReq = NULL;
ATA_Dev_Stat_t Status;
Int32 retVal = ATA_ERR_GEN;
if(NULL != pDevice)
{
retVal = ATA_NO_ERR;
pReq = ATA_AllocReq (pDevice, False);
if (pReq != NULL)
{
pReq -> MediaHandle = NULL;
pReq -> IsInternal = True;
pReq -> Command . Device = pDevice -> Dev;
pReq -> Command . Cmd = ATA_READ_MAX_SECT;
pReq -> Buffer = NULL;
pReq -> Mode = TASKFILE;
pReq -> Res . IsEvent = False;
pReq -> Handler = &ATA_IdentHndlr;
pReq -> ToHndlr = &ATA_IdentHndlr;
pReq -> Timeout = ATA_ONESEC_TO;
pReq -> Retry = 10u;
ATA_SubmitReq (pDevice, pReq);
while (pReq -> Retry != 0)
{
m_delay(1u);
}
Status = pReq->Status;
So how the value of pReq -> Retry changed?