Hi,
I have questions about AM335x.
Q1. My customer want to use LCD_DATA[15:8] as LCD I/F.
But they also want to use these pin as GPMC_A[19:12].
So, it is conflicting.
Is there any solution to realize LCD_DATA[15:8] and GPMC_A[19:12] function simutaneouly?
Is it available to use GPIO for LCD_DATA[15:8] function?
Q2.AM335x has a few UART ports but UART1 is only port which support DCDN/DSRN/DTRN/RIN signal.
My customer need 3 UART ports which support DCDN/DSRN/DTRN/RIN signal.
So, we are searching for the solution to realize these signal.
Are these signals(DCDN/DSRN/DTRN/RIN) feasible by GPIO?
best regards,
g.f.